2014-11-20 9:41 PM
Need help in understanding the
used by the STM32VLDISCOVERYboard.
The
http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/CD00161566.pdf
says the STM32 micro controller can be woken up by a raising edge. My interpretation is that the pull up resistor connected between the 3.3V and the wakeup pin will pull the wakeup pin high on power on. But I am not able to understand the use of the second resistor between the wake up pin and the ground. Will the two resistors not form a voltage divider circuit ? #stmvldiscovery2014-11-21 12:56 AM
There are two microcontrollers in the design!
Reviewing the STM32VLDISCOVERY schematics (MB913.pdf), R9 and R10 provide an analogue signal to AIN1 on the STM32F103C8T6 (U2 ST LINK).2014-11-21 10:56 AM
Thank you for explaining. However it will be helpful if you can explain the function of R1 and R2 in providing analog signal to the AIN1 on the STM32F103C8T6. As I understand R1 and R2 form a voltage divider circuit and pull down the voltage from 3.3V to 1.6V... However I am not able to understand the real intent of the resistors and the circuit they form.
2014-11-24 6:25 AM
I imagine it is just to let the ST Link microcontroller monitor the +3V3 supply voltage. The signal is marked as AIN_1 so it's going to be input to the microcontroller's internal A to D converter ADC1. The potential divider just reduces the voltage from +3V3 to about half that so that it's within the ADC range (typically 0 .. +2.5V in these systems).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.