2008-10-01 6:19 AM
Cortex -- PD0 interrupt
2011-05-17 3:26 AM
Hello,
I have a problem to configure PD0 as an input, interrupt enable. I got no external interrupts. Only software interrupt works. The GPIOD -- IDR (input data register) register shows the current state of this line. When I press to switch (PD0), The IDR register shows the 0 at PD0, otherwise it shows 1. So, it should generate an interrupt. I have other switches on other inputs and it works pretty well. Is there any examples to use PD0 and external interrupt? GPIO_PinRemapConfig(GPIO_Remap_PD01, ENABLE); EXTI_InitStructure.EXTI_Line = EXTI_Line0; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising_Falling; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); // Set the Preemption Priority to ''1'' NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; // Set the Command to ''Enable'' NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; // Configure and enable EXTI0 IRQ Channel NVIC_InitStructure.NVIC_IRQChannel = EXTI0_IRQChannel; NVIC_Init(&NVIC_InitStructure);2011-05-17 3:26 AM
Thank you very much, I have a 48 pin package... :(
2011-05-17 3:26 AM
Gives there a solution for this problem?
I have the same problem.2011-05-17 3:26 AM
RM0008, page 107: ''PD0, PD1 cannot be used for external interrupt/event
generation on 36, 48, 64-pin packages.''2011-05-17 3:26 AM
tibo-
Thank you from my firm too - we had started laying out a 64 pin device - even after having read/noted RM0008. Looks like its time to extract every ''gotcha'' to a special file where we're less likely to ''miss them'' in the mix...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.