2016-04-26 4:56 AM
Recent StCube device headers for F401 and F411 define Core coupled RAM for these devices. However datasheet/reference manual does not indicate existance of CCM RAM:
stm32f401xc.h:#define CCMDATARAM_BASE ((uint32_t)0x10000000U) /*!< CCM(core coupled memory) data RAM(64 KB) base address in the alias region */ stm32f401xc.h:#define RCC_AHB1ENR_CCMDATARAMEN ((uint32_t)0x00100000U) So either the headers or datasheet and reference manuals need update.2016-04-26 6:26 AM
I think it has more to do with the lineage of the files and the core. I'm not aware that the 401 has any CCMRAM
May be you want to focus on functional defects, rather than defines that haven't been purged from every member of the F4 family offering a subset of function to the others.2016-04-26 6:54 AM
Hi bonnes.uwe,
Thank you for your feedback. The issue has been reported internally.-Syrine-2016-04-27 3:16 AM
My work on the ethernut cross device cooperative RTOS
http://www.ethernut.de/ found in SVN HEAD https://sourceforge.net/projects/ethernut/files/ tries to rely on the device header as much as possible. With wrong devices defining CCM, I need to manual add items in the configurator to decide if a linker script using CCM can be offered, So perhaps you understand why I report these flaws in the device headers.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.