2017-09-04 12:16 AM
Hello,
I had a problem with my UART interface on STM32F091RC. I have seen that others encountered the same, but I am not able to fix yet in my side.
I have UART Rx and Tx in DMA normal mode.
Tx function is working fine (with long running test). But my Rx is stopping just after some random times (10s and 5 min or 2 min). And it is not tiggered any other interrupt !
I am using the code generated by Cube Mx.
void MX_USART2_UART_Init(void)
{huart2->Instance = USART3;
huart2->Init.BaudRate = 115200; huart2->Init.WordLength = UART_WORDLENGTH_8B; huart2->Init.StopBits = UART_STOPBITS_1; huart2->Init.Parity = UART_PARITY_NONE; huart2->Init.Mode = UART_MODE_TX_RX; huart2->Init.HwFlowCtl = UART_HWCONTROL_NONE; huart2->Init.OverSampling = UART_OVERSAMPLING_16; huart2->Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; huart2->AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; if (HAL_UART_Init(huart2) != HAL_OK) { //Error_Handler(); }}void HAL_UART_MspInit(UART_HandleTypeDef* uartHandle)
{GPIO_InitTypeDef GPIO_InitStruct;
if(uartHandle->Instance==USART3) { /* Peripheral clock enable */ __HAL_RCC_USART3_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE();/**USART2 GPIO Configuration
PA2 ------> USART2_TX PA3 ------> USART2_RX */ GPIO_InitStruct.Pin = GPIO_PIN_10|GPIO_PIN_11; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.Alternate = GPIO_AF4_USART3; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);/* Peripheral DMA init*/
hdma_usart2_rx->Instance = DMA1_Channel1;
hdma_usart2_rx->Init.Direction = DMA_PERIPH_TO_MEMORY; hdma_usart2_rx->Init.PeriphInc = DMA_PINC_DISABLE; hdma_usart2_rx->Init.MemInc = DMA_MINC_ENABLE; hdma_usart2_rx->Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE; hdma_usart2_rx->Init.MemDataAlignment = DMA_MDATAALIGN_BYTE; hdma_usart2_rx->Init.Mode = DMA_NORMAL; hdma_usart2_rx->Init.Priority = DMA_PRIORITY_LOW; if (HAL_DMA_Init(hdma_usart2_rx) != HAL_OK) { //Error_Handler(); }__HAL_DMA1_REMAP(HAL_DMA1_CH1_USART3_RX);
uartHandle->hdmarx = hdma_usart2_rx;
hdma_usart2_rx->Parent = uartHandle; __HAL_LINKDMA(uartHandle, hdmarx, *hdma_usart2_rx);hdma_usart2_tx->Instance = DMA1_Channel4;
hdma_usart2_tx->Init.Direction = DMA_MEMORY_TO_PERIPH; hdma_usart2_tx->Init.PeriphInc = DMA_PINC_DISABLE; hdma_usart2_tx->Init.MemInc = DMA_MINC_ENABLE; hdma_usart2_tx->Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE; hdma_usart2_tx->Init.MemDataAlignment = DMA_MDATAALIGN_BYTE; hdma_usart2_tx->Init.Mode = DMA_NORMAL; hdma_usart2_tx->Init.Priority = DMA_PRIORITY_LOW; if (HAL_DMA_Init(hdma_usart2_tx) != HAL_OK) { //Error_Handler(); }__HAL_DMA1_REMAP(HAL_DMA1_CH4_USART3_TX);
uartHandle->hdmatx = hdma_usart2_tx;
hdma_usart2_tx->Parent = uartHandle; __HAL_LINKDMA(uartHandle, hdmatx, *hdma_usart2_tx);/* Peripheral interrupt init */
HAL_NVIC_SetPriority(USART3_8_IRQn, 0, 0); HAL_NVIC_EnableIRQ(USART3_8_IRQn); }}void USART3_8_IRQHandler(void)
{ // If Overrun flag is still set, clear it if (__HAL_UART_GET_FLAG(huart2, UART_FLAG_ORE) != RESET) { __HAL_UART_CLEAR_OREFLAG(huart2);// Clear the buffer to prevent overrun
__HAL_UART_SEND_REQ(huart2, UART_RXDATA_FLUSH_REQUEST); }HAL_UART_IRQHandler(huart2);
}I just added the overrun test here in cube mx base code. But even if I remove it still have the same issue on Rx function.
Here all DMA channels are setting up.
void MX_DMA_Init(void)
{ /* DMA controller clock enable */ __HAL_RCC_DMA1_CLK_ENABLE();/* DMA interrupt init */
/* DMA1_Ch1_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Ch1_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Ch1_IRQn); /* DMA1_Ch2_3_DMA2_Ch1_2_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Ch2_3_DMA2_Ch1_2_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Ch2_3_DMA2_Ch1_2_IRQn); /* DMA1_Ch4_7_DMA2_Ch3_5_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Ch4_7_DMA2_Ch3_5_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Ch4_7_DMA2_Ch3_5_IRQn);}Here are the IRQ handler functions.
void DMA1_Ch1_IRQHandler(void)
{ HAL_DMA_IRQHandler(hdma_usart2_rx);}void DMA1_Ch4_7_DMA2_Ch3_5_IRQHandler(void)
{ HAL_DMA_IRQHandler(hdma_usart2_tx);}Would it be possible if someone can tell me what I am doing wrong in this code ?
Since 2 days I debugged this stuff without success.
Thanks a lot for your support.
2017-09-07 12:04 AM
Any help on this ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.