2012-07-06 1:02 AM
Hi,
With a STM32, I have a problemto select
either
EEPROM
(
M24LR64-R and M24M02-DR)on the same bus
I2C
.Here are the
''device
select
code
'':For
M24LR64
-R: 1 0 1 0 X 1 1 XIn the order
: 1 0 1 0 = Device type identifier X = E2 1 1 = E1 E0 ( chip enable) X = RWFor
M24M02
-DR:1 0 1
0 1
X
X
X
In the order
: 1 0 1 0 = Device type identifier 1 = E2 ( chip enable) X X = A17 A16 (MSB address bits ) X = RWThe two
address bits
A17
and
A16
for
M24M02
-DRcan not be
used
because they would
pose
a conflict with the
R
-
M24LR64there is
there a way
around the problem
?Thank you for your
response
, #pounds-head-on-desk2012-07-06 2:19 AM
there is
there a way
around the problem
? Due to the lack of forethought by ST the only way around it would be to use two I2C buses, or gate the clock between the two devices.2012-07-09 5:32 AM
there is
there a way
around the problem
?
yes, there is a plethora of I²C EEPROMS with 'pinnable' addresses (i.e. you change the address by grounding certain pins) change one or both to such. Erik
2012-07-09 6:32 AM
For my understanding, the E0,E1 pins of the
M24LR64-R
serve as address selection pins, thus allowing for 4 devices on one I2C bus. To cite the datasheet (CD00217247.pdf): 2.3 Chip Enable (E0, E1) These input signals are used to set the value that is to be looked for on the two least significant bits (b2, b1) of the 7-bit device select code. These inputs must be tied to VCC or VSS, to establish the device select code as shown in Figure 3. When not connected (left floating), these inputs are read as low (0,0). ... 5.5 Memory addressing To start communication between the bus master and the slave device, the bus master must initiate a Start condition. Following this, the bus master sends the device select code, shown in Table 2 (on Serial Data (SDA), most significant bit first). The device select code consists of a 4-bit device type identifier, and a 3-bit Chip Enable “Address�? (E2, E1, E0). To address the memory array, the 4-bit device type identifier is 1010b. Up to four memory devices can be connected on a single I2C bus. Each one is given a unique 2-bit code on the Chip Enable (E0, E1) inputs. When the device select code is received, the device only responds2012-07-09 6:45 AM
I'm going with Jonathan's analysis that these babies clash. I looked at the datasheets, he's probably wired them up.
Whoever thought putting high order address bits for the memory array into the I2C's device address needs to be tarred and feathered.2012-07-09 7:17 AM
Whoever thought putting high order address bits for the memory array into the I2C's device address needs to be tarred and feathered.
correction Whoever designs without reading datasheets fully needs to be tarred and feathered. The specific reason for the chips with the high order byte address in the I²C address is that these chips solely are intended as one chip replacements for 4 chips that have 1/4 the capacity and are address tied as the replacement chip reads them. For new development there are chips available with single I²C address and two byte byte address. Erik
2012-07-09 7:54 AM
For new development there are chips available with single I²C address and two byte byte address.
Or three byte addresses hopefully.2012-07-09 9:11 AM
Or three byte addresses hopefully.
really ''enough bytes to cover the capacity, hopefully'' two byte address will cover most (<65k bytes) Erik
2012-07-10 3:19 AM
ok,
thank youfor
your answers
but
we need
an
EEPROM
of 2Mb
and
a
radio EEPROM
We have not
found other
EEPROM
...
an idea?2012-07-10 3:52 AM
ST's implementation of the I2C controller is so awkward that you may end up ''bit-bashing'' the I2C on GPIO pins anyway. Do you have one (use as alternate I2C clock) or two (new I2C bus) spare pins? If not, you must multiplex the I2C bus you have. There are various buffer ICs etc. that might help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.