2011-02-14 7:40 AM
Common #define between linker and source code
2011-05-17 5:24 AM
You may need a separate program to do this. Perl should work nicely.
Put the address on the perl command line access with $ARGV[0]. Create two files. One for C; the other to include in your linker script. Or you could have perl find the address in your .h file and then create the include for the linker.2011-05-17 5:24 AM
Is there some other way to do what I need to?
Not 100% sure of your goal, but I've always used the fact I can export the address of the vector table (__Vectors), and used that to program the NVIC. Where it goes then depends on where you tell the Linker to put the object code. AREA RESET, DATA, READONLY EXPORT __Vectors __Vectors DCD __initial_sp ; Top of Stack DCD Reset_Handler DCD NMIException DCD HardFaultException DCD MemManageException ... extern void * __Vectors; NVIC_SetVectorTable((u32)(&__Vectors), 0x0); // Smart Base Location2011-05-17 5:24 AM
Clive
Thanks so much! That's exactly what I was looking for! I needed this for 2 things: a) initialization of the NVIC table (we change its allocation when we start application code from our boot sector) and b) a self-imposed ''stack size checker'' routine that we generated that uses stack start address in the NVIC table to place a word near the top of the stack that we periodically check for corruption (pointing to a stack overflow issue). defining the NVIC table address externally in the linker file did the trick, THANKS!2011-05-17 5:24 AM
I like my code to be as agnostic as possible to the address it compiles/runs at. And where it matters, to just have one symbol to reference, and not rely on changing multiple settings or defines that subsequent maintainers might overlook.
Well you could add startup code to pre-fill the stack with a initialization pattern, and then monitor how deep it actually gets. This can be examined periodically, or within a JTAG memory view window. You also place a magic word at the maximal extent (SP - 0x1FC, for example) and periodically monitor that for corruption. This is probably what you were talking about, I'd probably refer to it as the bottom of the stack as it is descending.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.