2008-02-21 7:08 AM
cofiguring Rowley CrossWorks to work with DFU
2011-05-17 3:24 AM
never mind - figured it out
1.http://ccgi.rowley.co.uk/support/faq.php?do=article&articleid=52
2. memory map file (in C:\Program Files\Rowley Associates Limited\CrossWorks for ARM 1.7\targets\ST_STM32F10x) for the processor has to be modified with correct settings for FLASH area (start at 0x08003000, length....) 3. call to vector table needs to be NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x3000);2011-05-17 3:24 AM
K, here is the situation.
I am attempting to create DFU (ST Micro) compatible application that suppose to run on STM3210xx device using Rowley v 1.7 toolchain. DFU loader already in flash and recognized by DFU demo software. I also created small GPIO application (based on GPIO example that came with Crossworks) that toggles some LEDs on the demo board ( board is OIMEX STM32-P103) Application compiles, load via JTAG and runs fine. Now I want to be able to load that application into the flash using DFU. I have modified NVIC_Configuration(void) to: ///////////////////////////////////////////////////////////////////////////////////////// void NVIC_Configuration(void) { NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x3000); } //////////////////////////////////////////////////////////////////////////////////////////// created .dfu file, load it - doesn't run I also tried: in flash_placement.xml change FLASH-vectors->start address to 0x08003000 loads, doesn't run In both cases computer comes up with USB device not recognized ( not surprising there is no USB code in downloaded app) but LEDs dont' blink. DFU application still in the memory and still loads when ''boot'' button is pressed upon power up. So question is how do you configure CrossWorks to produce DFU compatible executable? Thank you MikeWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.