2008-03-20 12:42 AM
CodeSourcery STM32 build environment
2011-05-17 3:22 AM
Which, as far as I can tell, is now at
https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/ARM CortexM3 STM32/STM32 CC%2B%2B build environment using CodeSourcery Sourcery G%2B%2B¤tviews=18152
after a URL scheme change2011-05-17 3:22 AM
Here's an open and ready to use build environment for the STM32. Enjoy!
CodeSourcery/STM32 (Lanchon 1-Feb-2008) This is an STM32 build environment for CodeSourcery arm-2007q3-53-arm-none-eabi. The GCC version of the STM32F10x Firmware Library 1.0 (10/08/2007) is included in full and unchanged. Startup code is taken form this library. Linker scripts are taken from the RAISONANCE RKitARM for RIDE7 1.03.0004. The scripts have notes permitting use: ''Copyright RAISONANCE 2007. You can use, modify and distribute this file freely, but without any warranty.'' We should all be thankful to them. Please consider RAISONANCE's RIDE7 if you need an advanced IDE. Included is a demo project that flashes a led connected to PC12 (ready to run on an Olimex STM32-H103 board). To build it change to the project directory and use the make tool that came with CodeSourcery: cs-make to build the firmware library and the main application cs-make -B to force a complete rebuild cs-make clean to delete all previously built object files cs-make flash to flash an STM32 after building via JTAG using OpenOCD Configuration is done through these files: makefile build options (optimization, etc) stm32.ld target memory size and type stm32f10x_conf.h firmware library configuration stm32f10x_it.c interrupt handlers jtag/flash.cfg OpenOCD configuration (JTAG dongle, etc) To flash you need OpenOCD installed. See openocd.berlios.de (or www.yagarto.de for a win32 port). Cheers! [ This message was edited by: lanchon on 01-02-2008 09:22 ]2011-05-17 3:22 AM
I touched the makefile today, now it has better build options and the firmware library is built with different options than the rest of the app. (I never use make so somebody should take a look.)
2011-05-17 3:22 AM
I just found out that some people continue to use this and are having trouble.
to make it clear: this was deprecated in favor of .2011-05-17 3:22 AM
http://www.codesourcery.com/sgpp/lite/arm/portal/subscription?@template=lite
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.