2015-11-26 7:38 AM
Good Evening,
Does anyone have a working example for transfer of multiple bytes over SPI between 2 STM32 using Interrupts and NSS_Hard ? I have tried coding both the Master and Slave Side. Both are receiving and transmitting data but there is no synchronization and garbage value is received. I have taken care that NSS is low during transfer and high otherwise. On scope , I see data those garbage data. But I really cannot figure out where I am getting out of Sync. If someone could provide me the code , I would be very grateful. Regards #stm32f4 #device #spi #discoveryWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.