2016-02-04 11:41 AM
Hello!
I am running tests on an SD card plugged into my STM32F746G-Discovery board. I am using the STM32F7xx_HAL_Driver and the BSP utilities provided for the Discovery board to access the SD card.When I use DMA for transfers to the SD card (BSP_SD_WriteBlocks_DMA()
), everything works as expected and the tests pass without error. However, when I transfer in polling mode (BSP_SD_WriteBlocks()
), after a few hundred I/O operations, I run into the following error: inHAL_SD_WriteBlocks()
, after issuing a CMD16 (SD_CMD_SET_BLOCKLEN
), I get a command timeout error (SD_CMD_RSP_TIMEOUT
). If I backup and try the CMD16 again, it timeouts again (even if I try 50 times).This problem happens on multiple SD cards. The error does not occur in the same place every time; it may be on the 420th iteration or the 460th (etc), but it does happen every time I run through the tests. Is this a hardware issue? Or a driver bug? Or possibly a configuration problem on my part? #stm32f746discovery-sd-card #sdio-sdhc-stm32 #stm32f72016-02-04 1:16 PM
I'm also getting the same error (timeout after CMD16) from BSP_SD_ReadBlocks() when using FatFs with the SD driver provided by ST Micro (sd_diskio.c). Again, it doesn't happen at a predictable time; many reads pass successfully before it fails.
So it's looking like this is an issue with either the board or the driver.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.