2020-08-19 4:21 AM
Hello,
I have problem with CRS (Clock recovery system) in STM32F091xx. I use HSI48 and I want to generate synchronization with LSE (32.768 kHz).
How to set FELIM in CFGR register and TRIM in CR register ?
Thank your for help.
Solved! Go to Solution.
2020-08-19 5:58 AM
Set RELOAD and FELIM fields accordingly in the CRS_CFGR register.
RELOAD = (fTARGET / fSYNC) - 1
FELIM = (fTARGET / fSYNC) * STEP[%] / 100% / 2
For you, fTARGET=48MHz, fSYNC=32kHz, and STEP=0.14%.
TRIM is adjusted automatically. You don't set it manually.
2020-08-19 5:58 AM
Set RELOAD and FELIM fields accordingly in the CRS_CFGR register.
RELOAD = (fTARGET / fSYNC) - 1
FELIM = (fTARGET / fSYNC) * STEP[%] / 100% / 2
For you, fTARGET=48MHz, fSYNC=32kHz, and STEP=0.14%.
TRIM is adjusted automatically. You don't set it manually.
2020-08-19 11:15 AM
Thank you for help !
2022-07-20 10:17 AM
It is best to keep in mind that the intended fSYNC target is around 1kHz based on the USB SOF. This yields a FELIM of 34 which CubeMX defaults to. Using fSYNC=32768 causes FELIM to be 2 which is a very small margin and causes CRS to auto trim much more frequently than intended. I am using LSE/32 for fSYNC=1024 and FELIM of 33 based on the equations above.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.