2016-03-28 6:21 AM
Hi STM,
As part of our project we are using STM32F411RET6 series MCU, We have followed clock configuration from the below link http://www.st.com/web/en/catalog/tools/PF257927 As Maximum clock for the MCU what we are using is 100Mhz. And our requirement is * mcu has run at 100Mhz or (Maximum clock) * We are using SPI peripheral and TIM7 in which both are using APB1 clock . below are clock configuration we are using and we have on board external 26Mhz crystal oscillator cpu_clock : 100000000 HSE_SOURCE : RCC_HSE_ON AHB clock divder : RCC_SYSCLK_Div1 APB1 clock divder : RCC_HCLK_Div4 APB2 clock divder : RCC_HCLK_Div2 Pll source : RCC_PLLSource_HSE PLLM : 13 PLLN : 200 PLLP : 4 PLLQ : 9 System clock source : PLL clock systick clock source : SysTick_CLKSource_HCLK Internal flash wait state : 3 cycles Below is my Brief understanding about the configuration cpu clock is at 100 Mhz AHB clock at 100 Mhz APB1 clock at 100/4 = 25 Mhz APB2 clock at 100/2 = 50 Mhz Please let me know my understanding is right. Now Question is, from clock configuration tool if Cpu clock is running at 100 Mhz( possible max speed ) max APB1 clock is 36Mhz from above configuration APB1 is 25Mhz, which is impacting throughtput of SPI periphral what we are using. And at the same time we are using TIM7 for internal monitoring purpose. Is there any way to bump up the APB1 clocks so that it can run at its maximum speed(36Mhz). From clock configuration tool if cpu_clock is 72Mhz then APB1 is running at is maximum speed i.e., 36Mhz, but we dont want cpu clock to run at lower speed. Please provide us a solution which unblocks us. Please let me know if any more data needed. Thanks & Regards, Teja. #clock-configuration2016-03-28 8:32 AM
Data sheet shows APB1 capable of 50 MHz operation. (Fig 3, Pg 15)
http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00115249.pdf
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.