2008-07-29 9:55 PM
Check of ADC-EOC Flag
2011-05-17 3:40 AM
Hi,
I'd like to wait until the end of an AD-conversion before I read out the data-register. But the EOC-flag is not set?!? My configuration is: { ADC1->SQR1 &= ~0x00F00000; // only one conversion, clear L-Bits /* sampletime 7.5 cycle for CH14 */ ClrBit(ADC1->SMPR1,14); ClrBit(ADC1->SMPR1,13); SetBit(ADC1->SMPR1,12); ADC1->SQR3 = 0x0000000E; //set CH4 for first conversion ADC1->CR1 = 0x00000000; //control configuration ADC1->CR2 |= 0x000E0000; //triggered by software SetBit(ADC1->CR2,0); //Set ADON to enable ADC SetBit(ADC1->CR2,22); //Set SWS to start conversion while(!CheckBit(ADC1->SR,1)); //Check EOC-flag and wait until conversion is complete return(ADC1->DR) } When I uncomment the ''while...'' line it works fine... Otherwise the programm stops here. What is wrong? Michael2011-05-17 3:40 AM
Hi,
I believe that this coming from the set of ADON bit sequence where the software has to wait a stabilization time before triggering other conversions. I found on RM0008 this description : Bit 0 ADON: A/D Converter ON / OFF This bit is set and cleared by software. If this bit holds a value of zero and a 1 is written to it then it wakes up the ADC from Power Down state. Conversion starts when this bit holds a value of 1 and a 1 is written to it. The application should allow a delay of tSTAB between power up and start of conversion. Refer to Figure 22. 0: Disable ADC conversion/calibration and go to power down mode. 1: Enable ADC and to start conversion Note: If any other bit in this register apart from ADON is changed at the same time, then conversion is not triggered. This is to prevent triggering an erroneous conversion. I suggest you to add a delay between : SetBit(ADC1->CR2,0); //Set ADON to enable ADC delay (time); SetBit(ADC1->CR2,22); //Set SWS to start conversion And check if it is working. Note that reading the DR in the next instruction will automatically clear the EOC bit. Cheers, STOne-32.2011-05-17 3:40 AM
Hello,
thanks for your suggestion! You are right. It is due to setting the ADON-Bit the right way. In my previose ADC-calibration routine I cleared the ADON-Bit at the end, so the ADC fell to sleep again and I have to set the ADON-Bit to times for the next conversion. I left to set the SWS-Bit because when I set the ADON-Bit the second time (when the ADC is powered up) a conversion is triggered. So do I need to set the SWS-Bits in this application? Cheers and thank you for your support!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.