2012-08-21 10:45 AM
Hi all,
I use STM32F205xx for my project but I did the same results with STM32VL Discovery kit. I debug in Atollic TrueSTUDIO 2.3.0 Lite and I tried TrueSTUDIO 3.1. too. The problem is that code char a = -50; short b = a; does cast negative values correctly. Internal representation of char should be signed and therefore b variable should be -50 and not 206, which is the result. I checked this in VisualStudio and the result was -50 as expected. Another brand controller does it as expected. I checked also disassembly listing. The code for other controller uses signed extend of data for this cast. Atollic makes a simple copy without signed extension. Do I understand something wrong or is it a problem of a compiler? How to deal with it correctly? Is it about settings of the compiler? Thank you for your reactions in advance2012-08-21 11:38 AM
Probably because GCC thinks 'char' is 'unsigned char' by default.
The standard does not specify if plainchar is signed or unsigned.
Check the values of CHAR_MIN and CHAR_MAX as defined in limits.h, and if __CHAR_UNSIGNED__ is defined or not.
http://www.linuxtopia.org/online_books/an_introduction_to_gcc/gccintro_html
2012-08-22 3:29 AM
Thank you for the quick reply.
Yes, I expected char to be specified as signed, but it is not. So I will continue using ''signed char'' type declaration instead of ''char'' Btw. when calling a functions like this, the compiller warns me about difference in signednes. void function (char * c);
unsigned char aaa;
function (&aaa);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.