2016-03-22 8:48 AM
Are you kidding?
What sense has this function made in this way ?uint8_t CDC_Transmit_FS(uint8_t* Buf, uint16_t Len){ uint8_t result = USBD_OK; /* USER CODE BEGIN 7 */ USBD_CDC_SetTxBuffer(hUsbDevice_0, Buf, Len); while(result != USBD_OK); <<<<<<<<<<<< i think useless do { result = USBD_CDC_TransmitPacket(hUsbDevice_0); } while(result != USBD_OK); /* USER CODE END 7 */ return result; <<<<<<<<<<< wath else can i return with >>while(result != USBD_OK);<<}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.