2020-11-19 3:44 AM
Hello Everyone ,
I'm working on project wich require using vl53l0x Sensor of STM32 B-L475E-IOT01 and i have one issue wich is I Cannot have a PWM signal in output when i'm using vl53l0x senor .
I have set a 80 MHz clock and i configured the Timer and all the registers to have a PWM signal in output and everything is working , but when i added the vl53l0x package , nothing is work even the sensor , in output i have 0 value ( testing the proximity) . So I decided to make sure if the package of the senor is working , I disabled the Timer and all the regesiters and in the output i have the right value of proximity .
So to simplify the things :
Only PWM in output : Working.
Only vl53l0x proximity value: Working.
PWM in output + vl53l0x proximity value : Both not working .
Anyone can help me please and Thank you .
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.