2020-05-04 5:51 AM
Can we use the reserved location of IVT as defined below 0x08000000
__vector_table
DCD sfe(CSTACK)
DCD Reset_Handler ; Reset Handler
DCD NMI_Handler ; NMI Handler
DCD HardFault_Handler ; Hard Fault Handler
DCD MemManage_Handler ; MPU Fault Handler
DCD BusFault_Handler ; Bus Fault Handler
DCD UsageFault_Handler ; Usage Fault Handler
DCD 0x08000000 ; Reserved
DCD 0 ; Reserved
DCD 0 ; Reserved
2020-05-04 6:43 AM
Yes. The CPU won't care about unused locations in the vector table as those interrupts should never get triggered.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.