2016-02-12 1:18 AM
Hi,
I'm using the STM32L053R8 on a Nucelo (L053R8) board and I can't seem to get anything on the TX line. It doesn't even get pulled high as you'd expect from the USART module before any transmission. I have the pin set correctly (as far as I can tell) but my oscilloscope hooked up to the TX pin has it at 0V at all times. Below is my full code. Note that I'm using MikroC for ARM however, aside from a few GPIO functions everything USART related involves direct register addressing so it should be pretty easy to follow if you aren't used to MikroC. Any help would be greatly appreciated. Cheers.
void main(){
// ------------------------- GPIO Control -------------------------- \\
// Set PORTA as digital output
GPIO_Digital_Output(&GPIOA_BASE, _GPIO_PINMASK_5); //Set LED as output
GPIO_Digital_Output(&GPIOA_BASE, _GPIO_PINMASK_2);
GPIO_Config(&GPIOA_BASE, _GPIO_PINMASK_2, _GPIO_CFG_PULL_UP);
// ------------------------- Clock Control ------------------------- \\
RCC_CR.PLLON = 0; // Disable PLL
RCC_CR.MSION = 1; // Enable MSI clock
// Set MSI clock to 5288 kHz
RCC_ICSCR.MSIRANGE0 = 1;
RCC_ICSCR.MSIRANGE1 = 1;
RCC_ICSCR.MSIRANGE2 = 0;
// Use MSI as system clock
RCC_CFGR.SW0 = 0;
RCC_CFGR.SW1 = 0;
RCC_CFGR.HPRE3 = 0; // AHB Prescaler - System Clock not divided: HCLK = System Clock = MSI = 0.524288 MHz
// Set APB2 prescar to 2: PCLK2 = HCLCK/2 = 0.262144 Mhz
RCC_CFGR.PPRE20 = 0;
RCC_CFGR.PPRE21 = 0;
RCC_CFGR.PPRE22 = 1;
// Set APB1 prescar to 2: PCLK1 = HCLCK/2 = 0.262144 Mhz
RCC_CFGR.PPRE10 = 0;
RCC_CFGR.PPRE11 = 0;
RCC_CFGR.PPRE12 = 1;
// Now enable peripheral clocks
RCC_IOPENR = 0b101; // Enable clock on PORTC & PORTA
RCC_IOPSMEN = 0b100; // Enable clock on PORTC & PORTA during sleep mode
RCC_APB2ENR.SYSCFGEN = 1; // Enable Peripheral Clock on SYSCFGEN (System configuration controller clock) - APB2 (0.262144 Mhz)
RCC_APB1ENR.USART2EN = 1; // Enable clock on USART2 - APB1 (0.262144 Mhz)
// ----------------------------- USART ----------------------------- \\
USART2_CR2 = 0;
USART2_CR3 = 0;
// Set USART2 clock as PCLK1 = 0.262144 Mhz
RCC_CCIPR.USART2SEL0 = 0;
RCC_CCIPR.USART2SEL1 = 0;
//Set USART2 Baudrate to 9600 with oversampling to 16
USART2_BRR = 0x1B; // 262144 / 9600 = 27 = 0x1B
USART2_CR1.OVER8 = 0;
// Set PORTA.2 as USART2-TX - Alternate Function 4
GPIOA_AFRL.AFSEL20 = 0;
GPIOA_AFRL.AFSEL21 = 0;
GPIOA_AFRL.AFSEL22 = 1;
GPIOA_AFRL.AFSEL23 = 0;
// Set PORTA.2 as USART2-RX - Alternate Function 4
GPIOA_AFRL.AFSEL30 = 0;
GPIOA_AFRL.AFSEL31 = 0;
GPIOA_AFRL.AFSEL32 = 1;
GPIOA_AFRL.AFSEL33 = 0;
// Configure USART word length (8), parity (none) and stop bits (1)
USART2_CR1.M0 = 0;
USART2_CR1.M1 = 0;
USART2_CR1.PCE = 0;
USART2_CR2.STOP0 = 0;
USART2_CR2.STOP1 = 0;
//Disable Flow Control
USART2_CR3.CTSE = 0;
USART2_CR3.RTSE = 0;
// Enable USART2 Module
USART2_CR1.UE = 1;
// Enable TX
USART2_CR1.TE = 1;
// Transmit some data
while(USART2_ISR.TXE == 0);
USART2_TDR = 'a';
while(USART2_ISR.TXE == 0);
// ----------------------- Main Program ---------------------------- \\
while(1){
GPIOA_ODR = 0b0000000000100000;
delay_ms(2000);
GPIOA_ODR = 0b0000000000000000;
delay_ms(2000);
}
}
#usart #stm32 #tx #transmission
2016-02-12 1:27 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.