2018-07-08 6:52 AM
Hello,
Thanks for all your wonderful support !
i read the full CAN section in RM of STM32F446RE but could not able to understand how CAN2 differs from CAN1, why CAN2 called as slave ?
its mentioned that , CAN2 cannot access SRAM
what exactly is the purpose of SRAM?. the RM has no discussion on this
is it like a shared memory between CAN1 and CAN2 ?
suppose if i want to receive a CAN message over CAN2, then once it passes acceptance filtering of CAN2 it comes to the FIFO of CAN2 and application reads it . where SRAM comes in to picture ?
Thank you for help.
#stm32f446reWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.