2018-11-15 11:31 AM
Hello,
I'm trying to use the STM32 MAT/TARGET to setup a Communication between Simulink and a STM32f107vct via CAN.
When I want to build the Simulink model i get an "INVALID INDEX" Block Diagram error.
I am using Matlab R2018b and the latest version of STM32CubeMx.
Do you have documentations concerning CAN setup with a virtual and a hardware channel in Simulink?
Thanks in advance for your answer.
Kind regards
Jens
2018-12-12 10:54 AM
Hi,
Mathworks are aware about the bug: https://nl.mathworks.com/support/bugreports/1895608?s_tid=srchtitle
Or more detailed for STM32-MAT:
The question is now who can implement this workaround in the toolchain?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.