2017-08-08 1:56 AM
I download the en.stm32cubemx.zip file from st.com website, but can't install it.
When I double-click the SetupSTM32CubeMX-4.22.0.app, nothing happen.
my java version is :
╰─
$
java -version
java version '1.8.0_111'
Java(TM) SE Runtime Environment (build 1.8.0_111-b14)
Java HotSpot(TM) 64-Bit Server VM (build 25.111-b14, mixed mode)
And the system OS is 10.12.6, should be the latest version.
2017-08-09 5:16 AM
Hi
guo.xinwen
,This is internally reported for review. We will keep you posted about any further update.
Khouloud.
2017-08-09 6:28 AM
been broken this way for many versions now. open a terminal window and cd into the installer's directory and
sudo java -jar SetupSTM32CubeMX-4.22.0.exe and it should install.
2017-08-14 2:11 AM
Thank you for your reply. I have install the application with your method. But when I startup the STM32CubeMX, the app will use a lot of CPU, seems like it is checking something as the 'Checking' button showing.
Can you help me fix this problem?
2017-08-14 2:12 AM
Installation is OK with the method of john dos, but there's still problem when I open the application. Why it is so hard to use it on the Mac OS?
2017-09-12 12:41 AM
Hello
guo.xinwen
,I would like first to thank you for your symptoms reporting.
This problem is link with a MacOSx new security feature.
You can refer to this links:
http://krypted.com/mac-security/app-translocation-services-os-x-10-12/
https://developer.apple.com/library/content/releasenotes/MacOSX/WhatsNewInOSX/Articles/OSXvhtml
When a zip, or dmg, is dowloaded from the web, an attribute is automatically added (
com.apple.quarantine).
Because of this, the execution is done in a sandbox context, underprivate/var/folder/xxxxx directory.
In case of cubemx, the app is launched in the sandbox, and it refer to ../../../Setupxxxx.exe file, which does not exist in the sandbox context -> thus file not found error (message reported in the console - system.log).
The workaround is to launch the installation by the java -jar command line.
We are looking if this behave can be avoided.
Kind regards
Sirma
2017-09-12 3:16 AM
I have installed the CubeMX by the java -jar method, but when I startup CubeMX, it will use lot of cpu, seems like it is checking update on the backgroud. And the checking will alway going on, no stop.
�自网易邮箱大师
在2017年09月12日 15:42,Sirma Siang<st-microelectronics@jiveon.com> 写�:
|
|
STMicroelectronics Community
|
|
You have been mentioned
by Sirma Siangin Re: can not install stm32cubemx on mac in STMicroelectronics Community - View Sirma Siang's reference to you
Hello guo.xinwen,
I would like first to thank you for your symptoms reporting.
This problem is link with a MacOSx new security feature.
You can refer to this links:
App Translocation Services In OS X 10.12 - krypted.com
macOS Sierra 10.12
When a zip, or dmg, is dowloaded from the web, an attribute is automatically added (com.apple.quarantine).
Because of this, the execution is done in a sandbox context, under private/var/folder/xxxxx directory.
In case of cubemx, the app is launched in the sandbox, and it refer to ../../../Setupxxxx.exe file, which does not exist in the sandbox context -> thus file not found error (message reported in the console - system.log).
The workaround is to launch the installation by the java -jar command line.
We are looking if this behave can be avoided.
Kind regards
Sirma
Participate in the conversation by replying to this email
This email was sent by STMicroelectronics Community because you are a registered user.
You may unsubscribe instantly from STMicroelectronics Community, or adjust email frequency in your email preferences
|
|
2017-09-12 6:52 AM
Have you settup your connection parameters ?
Enterring in Help->Updater Settings, does the Check Connection button is green (or a red cross appears) ?
KR
Sirma
2017-09-12 8:32 AM
If I click 'Updater Settings' button, CubeMx show the message box with 'Updater is already in use and checking Server. Then, please retry launching the updater after few seconds'
But the checking will not stop. and the 'Checking' button is gray, seems like checking is on going. You can see that in the attachment.
I am wondering if you have use the CubeMx on Mac. If on your computer, the program runs OK, I can try to reinstall it again.
�?�自网易邮箱大师
在2017年09月12日 19:52,Sirma Siang<st-microelectronics@jiveon.com> 写�?�:
|
|
STMicroelectronics Community
|
|
Re: can not install stm32cubemx on mac
reply from Sirma Siang in STM32 MCUs Forum - View the full discussion
Have you settup your connection parameters ?
Enterring in Help->Updater Settings, does the Check Connection button is green (or a red cross appears) ?
KR
Sirma
Reply to this message by replying to this email, or go to the message on STMicroelectronics Community
Start a new discussion in STM32 MCUs Forum by email or at STMicroelectronics Community
Following Re: can not install stm32cubemx on mac in these streams: Inbox
This email was sent by STMicroelectronics Community because you are a registered user.
You may unsubscribe instantly from STMicroelectronics Community, or adjust email frequency in your email preferences
|
|
________________ Attachments : �幕快照 2017-09-12 䞋�9.29.31.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HySA&d=%2Fa%2F0X0000000b7r%2FPDUkjMIn1lDOb6Fr2cWT7qsQjZ1I6HJkoLKmw2DtJHE&asPdf=false2017-09-13 12:58 AM
I am using an up to dated MacOSx machine.
Cube is running fine.
Delete the .app and reinstall it might be a good idea.
Kind regards
Sirma
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.