2011-03-13 10:24 PM
can not detect olimex STM32-H107 Virtual Port
2011-05-17 5:27 AM
Here is the schematic of Olimex STM32-H107 board
http://www.olimex.com/dev/pdf/ARM/ST/STM32-H107-schematic.pdf
Is R34 populated on your board?
The schematic shows it as NA
This resistor connects MCU PA9/OTG_FS_VBUS pin to the USB connector VBUS pin.
The OTG engine requires this connection to enable on-chip D+ pull-up resistor automatically at plug-in.
> the device is not detected on windows XP first
It suggests that the D+ pull-up resistor is not enabled.
So, I have doubt on the R34 resistor.
Tsuneo
2011-05-17 5:27 AM
Thanks for the reply,, You are right R34 is not populated. But, D+ pull-up resistor is connected to PA12 of MCU. I am setting this GPIO pin so that D+ pull-up resistor is enabled. Still, I could see that the device is not getting detected...
Is n't it the case that we can drive it without R34 also?
Thanks,
Sai
2011-05-17 5:27 AM
> But, D+ pull-up resistor is connected to PA12 of MCU.
This OTG engine has on-chip pull-up resistor(s). You don't need any external one.
> I am setting this GPIO pin so that D+ pull-up resistor is enabled. Still, I could see that the device is not getting detected..
Check the voltage of D+ and D- lines. Do you see the pull-up voltage at one of these lines?
As Windows don't tell any USB hardware connection, I believe these lines are kept in low.
Maybe, the connection routine, which enables the external pull-up, is not called on your firmware.
Did you change the processor type on the header file, as follows?
The default is STM32F10X_XL. For STM32F107, STM32F10X_CL is chosen.
Or, as the tips suggests, add this definition to the compile option.
----------------- excerpt from the source code, from here ----------------
\Libraries\CMSIS\CM3\DeviceSupport\ST\STM32F10x\stm32f10x.h
/* Uncomment the line below according to the target STM32 device used in your
application
*/
#if !defined (STM32F10X_LD) && !defined (STM32F10X_LD_VL) && !defined (STM32F10X_MD) && !defined (STM32F10X_MD_VL) && !defined (STM32F10X_HD) && !defined (STM32F10X_XL) && !defined (STM32F10X_CL)
/* #define STM32F10X_LD */ /*!< STM32F10X_LD: STM32 Low density devices */
/* #define STM32F10X_LD_VL */ /*!< STM32F10X_LD_VL: STM32 Low density Value Line devices */
/* #define STM32F10X_MD */ /*!< STM32F10X_MD: STM32 Medium density devices */
/* #define STM32F10X_MD_VL */ /*!< STM32F10X_MD_VL: STM32 Medium density Value Line devices */
/* #define STM32F10X_HD */ /*!< STM32F10X_HD: STM32 High density devices */
// #define STM32F10X_XL /*!< STM32F10X_XL: STM32 XL-density devices */ // <------ comment this line
#define STM32F10X_CL /*!< STM32F10X_CL: STM32 Connectivity line devices */ // <------ recover this line
#endif
/* Tip: To avoid modifying this file each time you need to switch between these
devices, you can define the device in your toolchain compiler preprocessor.
----------------- to here ----------------
Tsuneo
2011-05-17 5:27 AM
Tsueno,
I could have the USB port working by putting PA11 and PA12 to BIT_RESET. You are right that those pull-up resisters are inside OTG. As the lines are multiplexed between PA11/USART/OTG_FS_DP, i disabled PA11 (and USART lines are not connected on this board), so that connected OTG_FS_DP to D+. So, I could detect it finally and Windows Recognizes it as Virtual COM port..
The tool chain I am using(CrossWorks) automatically selects STM32F10X_CL as build option for STM32F107.
I have different set of problems now.. I will post a different topic for that..
Thanks,
Sai
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.