2018-08-20 3:30 AM
Please tell me how to send a CAN message using HAL_CAN_Transmit function.
For ex. if I want send a hex number say 0xFE.
2018-08-20 5:15 AM
i use the cube to initialise all the peripherals with HAL. including CanBus
but it ends there,
I use this to transmit.
if ((CAN->TSR & CAN_TSR_TME0) == CAN_TSR_TME0) // (1) fifo0 is empty
{
CAN->sTxMailBox[0].TDTR = 8; // (2) length
CAN->sTxMailBox[0].TDLR = 0x11223344; // (3) 4bytes
CAN->sTxMailBox[0].TDHR = 0x44556677; // (3) 4bytes
CAN->sTxMailBox[0].TIR = ((uint32_t)TxMsgID << 21 | CAN_TI0R_TXRQ); // (4)
// sent to fifo now, if the line is idle it will start now
}
if ((CAN->TSR & CAN_TSR_TME1) == CAN_TSR_TME1) // (1) fifo1 is empty
{}
if ((CAN->TSR & CAN_TSR_TME2) == CAN_TSR_TME2) // (1) fifo2 is empty
{}
2018-08-20 5:42 AM
Perhaps looks at some code examples for the STM32 part you're using?
STM32Cube_FW_L4_V1.12.0\Projects\STM32L476G-EVAL\Examples\CAN\CAN_Networking\Src\main.c
/* Set the data to be transmitted */
TxData[0] = 0xFE;
/* Start the Transmission process */
if (HAL_CAN_AddTxMessage(&CanHandle, &TxHeader, TxData, &TxMailbox) != HAL_OK)
{
/* Transmission request Error */
Error_Handler();
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.