2021-02-16 12:52 PM
I purchased a controller board from HiWonder, who use your STM32 MCU. I asked them if I can use python to program the STM32 but they do not know. Can I use python to program your microcontroller? Do I need to download specific software?
2021-02-16 1:18 PM
Well it definitely doesn't run python natively..
There are ports of Micro Python, likely not for random boards though.
2021-02-22 6:28 AM
Hi @SMeza.1 ,
To complete the answer provided by @Community member , you can look to the STM32 boards already supported in MicroPython. And the list of all available firmware is in this link.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-02-22 7:35 AM
Look also at this - it runs Python (not micro python though, their own brew)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.