2013-11-27 6:13 AM
Hi eveveryone,
I met a very strange problem in STM32F103VC. I used PB8 and PB9 for CAN, PA6 and PA7 for 2 channel ADC. The CAN communication use interrrupt mode, ADC use query mode. If I only use CAN, it works well, any message in CAN bus will generate RX interrupt; and if only ADC, it works well, I can get the voltage. But if I make them work togother, the ADC works well, the CAN cannot goto RX interrupt, but if I send message to the CAN bus, the CAN can goto RX interrupt once.This is my code.//////////////////////////////////////////////void NVIC_Configuration(void)
{ NVIC_InitTypeDef NVIC_InitStructure; //??????? &sharpifdef VECT_TAB_RAM /* Set the Vector Table base location at 0x20000000 */ NVIC_SetVectorTable(NVIC_VectTab_RAM, 0x0); &sharpelse /* VECT_TAB_FLASH */ /* Set the Vector Table base location at 0x08000000 */ NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x0); &sharpendif NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1);// //enable USART interrupt NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); // /* Enable CAN1 RX0 interrupt IRQ channel */ NVIC_InitStructure.NVIC_IRQChannel = USB_LP_CAN1_RX0_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 2; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); //enable TIM2 interrupt NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 3; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /* //enable TIM3 interrupt NVIC_InitStructure.NVIC_IRQChannel = TIM3_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 4; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); */}/********* CAN Configuration*************************/void CAN_GPIO_Configuration(void){ GPIO_InitTypeDef GPIO_InitStructure; /* CAN Periph clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB | RCC_APB2Periph_AFIO ,ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE); GPIO_PinRemapConfig(GPIO_Remap1_CAN1,ENABLE); /* Configure CAN pin: RX */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU;//GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOB, &GPIO_InitStructure); /* Configure CAN pin: TX */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOB, &GPIO_InitStructure); }void CAN_Configuration(void){ CAN_InitTypeDef CAN_InitStructure; CAN_FilterInitTypeDef CAN_FilterInitStructure; CAN_GPIO_Configuration(); /* CAN register init */ CAN_DeInit(CAN1); CAN_StructInit(&CAN_InitStructure); /* CAN cell init */ CAN_InitStructure.CAN_TTCM = DISABLE; CAN_InitStructure.CAN_ABOM = DISABLE; CAN_InitStructure.CAN_AWUM = DISABLE; CAN_InitStructure.CAN_NART = DISABLE; CAN_InitStructure.CAN_RFLM = DISABLE; CAN_InitStructure.CAN_TXFP = ENABLE; CAN_InitStructure.CAN_Mode = CAN_Mode_Normal; CAN_InitStructure.CAN_SJW = CAN_SJW_1tq; CAN_InitStructure.CAN_BS1 = CAN_BS1_3tq; CAN_InitStructure.CAN_BS2 = CAN_BS2_2tq; CAN_InitStructure.CAN_Prescaler = 6; //1MHz if (CAN_Init(CAN1,&CAN_InitStructure) == CANINITFAILED) { } CAN_FilterInitStructure.CAN_FilterNumber=0; CAN_FilterInitStructure.CAN_FilterMode=CAN_FilterMode_IdMask; CAN_FilterInitStructure.CAN_FilterScale=CAN_FilterScale_32bit; CAN_FilterInitStructure.CAN_FilterIdHigh=0x0000; CAN_FilterInitStructure.CAN_FilterIdLow=0x0000; CAN_FilterInitStructure.CAN_FilterMaskIdHigh=0x0000; CAN_FilterInitStructure.CAN_FilterMaskIdLow=0x0000; CAN_FilterInitStructure.CAN_FilterFIFOAssignment=0; CAN_FilterInitStructure.CAN_FilterActivation=ENABLE; CAN_ITConfig(CAN1,CAN_IT_FMP0, ENABLE); CAN_FilterInit(&CAN_FilterInitStructure);}/************ ADC configuration ***************************/
void ADC_Configuration(void){ ADC_InitTypeDef ADC_InitStructure; GPIO_InitTypeDef GPIO_InitStructure;RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1 | RCC_APB2Periph_GPIOA | RCC_APB2Periph_AFIO, ENABLE); // If I disable this line, CAN will enter interrupt
RCC_ADCCLKConfig(RCC_PCLK2_Div6); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6|GPIO_Pin_7; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN; GPIO_Init(GPIOA, &GPIO_InitStructure); ADC_DeInit(ADC1); ADC_InitStructure.ADC_Mode = ADC_Mode_Independent; ADC_InitStructure.ADC_ScanConvMode = DISABLE; ADC_InitStructure.ADC_ContinuousConvMode = DISABLE; ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfChannel = 1; ADC_Init(ADC1, &ADC_InitStructure); ADC_Cmd(ADC1, ENABLE); ADC_ResetCalibration(ADC1); while(ADC_GetResetCalibrationStatus(ADC1)); ADC_StartCalibration(ADC1); while(ADC_GetCalibrationStatus(ADC1));}u16 ADC_GetVal(ADC_TypeDef * ADCx, uint8_t ADC_Channel){ u16 adc_val = 0; ADC_RegularChannelConfig(ADCx, ADC_Channel, 1, ADC_SampleTime_239Cycles5 ); ADC_SoftwareStartConvCmd(ADCx, ENABLE); while(!ADC_GetFlagStatus(ADCx, ADC_FLAG_EOC )); adc_val = ADC_GetConversionValue(ADCx); return adc_val;} #stm32-adc-can-interruptWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.