2015-06-15 12:25 PM
ghhhhhhhhhhhhk
#lmgtfy #can-bus #stm32f207 #can-prescale-and-quanta2015-06-18 11:19 AM
May be it's not the software? Step back, and think about how you're tackling and presenting the problem.
Document/diagram your board and connectivity, along with your test methodology and scope traces.2015-06-19 12:11 AM
w was checked can i device with oscilloscope and its sending something on PA11 and PA12, im using can converter i-7530 connected to PC, soo i cant check ESR reg on it, i can check it only on me device
2015-06-19 1:14 AM
i just check and i have Bit Dominant Error - 0x50, when i set prescaler <= 16 i have
Acknowledgment Error - 0x302015-06-19 4:29 AM
Then you should perhaps focus on getting some coherent baud rate settings. In the last code pasted that looked to be 31250 baud, based on the limited data I'm working with here.
2015-06-19 4:33 AM
For a 250Kbit/sec data rate I calculate the prescaler as:
clock = 120000000 / (1 + 6 + 8) = 8000000 (CAN clock ticks, sum of quanta)
prescale = clock / rate = 8000000 / 250000 = 32 Not clocking at 120 MHz
2015-06-19 4:34 AM
ok i will try it and write post ;] thx
2015-06-19 4:43 AM
I set prescaler like in your post 32 its to much?
2015-06-19 4:58 AM
I was responding to Jack's values....
For 250 kbps I'd use a prescaler of 8, presuming a 30 MHz APB1 (CAN) clock, and 15 time quanta2015-06-19 5:09 AM
eh i try almos all prescalers and still nothing, maybe its converter problem but i cant check it i think
2015-06-23 11:31 PM
his file configures the system clock as follows:
*============================================================================= *============================================================================= * Supported STM32F2xx device revision | Rev B and Y *----------------------------------------------------------------------------- * System Clock source | PLL (HSE) *----------------------------------------------------------------------------- * SYSCLK(Hz) | 120000000 *----------------------------------------------------------------------------- * HCLK(Hz) | 120000000 *----------------------------------------------------------------------------- * AHB Prescaler | 1 *----------------------------------------------------------------------------- * APB1 Prescaler | 4 *----------------------------------------------------------------------------- * APB2 Prescaler | 2 *----------------------------------------------------------------------------- * HSE Frequency(Hz) | 25000000 *----------------------------------------------------------------------------- * PLL_M | 25 *----------------------------------------------------------------------------- * PLL_N | 240 *----------------------------------------------------------------------------- * PLL_P | 2 *----------------------------------------------------------------------------- * PLL_Q | 5 *----------------------------------------------------------------------------- * PLLI2S_N | NA *----------------------------------------------------------------------------- * PLLI2S_R | NA *----------------------------------------------------------------------------- * I2S input clock | NA *----------------------------------------------------------------------------- * VDD(V) | 3.3 *----------------------------------------------------------------------------- * Flash Latency(WS) | 3 *----------------------------------------------------------------------------- * Prefetch Buffer | ON *----------------------------------------------------------------------------- * Instruction cache | ON *----------------------------------------------------------------------------- * Data cache | ON *----------------------------------------------------------------------------- * Require 48MHz for USB OTG FS, | Enabled * SDIO and RNG clock | *----------------------------------------------------------------------------- *============================================================================= ******************************************************************************I find it in system_stm32f2xx.h its normal settings?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.