2009-08-09 9:33 PM
CAN Bit Dom Error
2011-05-17 4:19 AM
I am using the CAN port with version 2.0.3 of the st firmware library with the keil compiler. When I setup the CAN port it works for about 2 seconds before I get the CAN Bit Dom Error. I have tested the hardware and CAN connection will another application and these work fine.
Is anyone else having this issue and any ideas how I could resolve it. Thanks Ian2011-05-17 4:19 AM
I found that I was the cause of the problem I'd started using the CAN TX pin as a output about 2 seconds after start my application.
2011-05-17 4:19 AM
Hi Iam,
I am working with STM32F103RBT6 at the moment for CAN Communication. My CAN is receiving the msg and it is fine. But as I transfer the msg it showing me Bit dominant Error and I really tried all possible solution. Please help me out.
Regards
Hitesh
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.