2023-03-27 6:48 AM
while (1)
{
/* USER CODE END WHILE */
uint32_t Page=0x000000C8; //0x08040000
uint32_t B =FLASH_BANK_2 ;
FLASH_PageErase(Page,B);
HAL_FLASH_Unlock();
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_ALL_ERRORS);
uint64_t d={0x1111111111111123};
volatile uint32_t flashaddresss =0x08040000; // give the address where we need
HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD,flashaddresss,d );
HAL_FLASH_Unlock();
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_ALL_ERRORS);
FLASH_PageErase(flashaddresss,B);//1
HAL_FLASH_Lock();
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
2023-03-27 7:11 AM
Probably shouldn't do it in a tight loop
Instrument code better.
Output success/failure codes.
Avoid using the debugger to step-thru.
Output progress and memory content to the console.
I'm sure the initial erase needs the flash memory unlocked.
Perhaps look at examples in the Cube/HAL directories for whatever STM32 you are using.
2023-03-27 7:22 AM
hi if you have any program like this please share ...
2023-03-27 7:37 AM
> uint32_t Page=0x000000C8;
Really? Which STM32 has 0xC8 = 200 flash pages per bank?
2023-03-27 10:07 AM
This is the THIRD post on the SAME topic
STM32Cube_FW_L5_V1.2.0\Projects\NUCLEO-L552ZE-Q\Examples\FLASH\FLASH_EraseProgram
2023-03-27 10:18 AM
//****************************************************************************
// Quick Rough STM32L5 Flash Example - sourcer32@gmail.com
//****************************************************************************
static uint32_t GetBank(uint32_t Addr)
{
#if 0 // Single Bank Device
return(FLASH_BANK_1);
#else // Dual Bank Device
uint32_t bank = 0;
if (Addr < (FLASH_BASE + FLASH_BANK_SIZE))
{
bank = FLASH_BANK_1;
}
else if (Addr < (FLASH_BASE + FLASH_BANK_SIZE*2))
{
bank = FLASH_BANK_2;
}
return(bank);
#endif
}
//****************************************************************************
#define FLASH_START_ADDRESS 0x08040000 // Unused spot for example
// Function to write data to the flash memory
// BYTE pointer, Size in BYTES, put what you want in a STRUCTURE
void write_flash(uint8_t *data, uint32_t size)
{
FLASH_EraseInitTypeDef EraseInitStruct = {0};
uint32_t addr = FLASH_START_ADDRESS; // 64-bit aligned
uint64_t value;
uint32_t PageError;
if (!size) return; // Empty request
size = (size + 7) & ~7; // Round up to 64-bit words
// Unlock the flash memory for writing
HAL_FLASH_Unlock();
// Clear any pending errors
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_ALL_ERRORS);
// Fill EraseInit structure, spanning size of write operation, within bank
EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES;
EraseInitStruct.Banks = GetBank(addr); // Bank
EraseInitStruct.Page = GetPage(addr); // Starting Page
EraseInitStruct.NbPages = GetPage(addr + size - 1) - EraseInitStruct.Page + 1; // Page Count, at least 1
if (HAL_FLASHEx_Erase(&EraseInitStruct, &PageError) != HAL_OK)
{
// Insert code to handle the error here
HAL_FLASH_Lock();
return;
}
size /= sizeof(uint64_t); // Byte count to 64-bit word count
// Iterate over the array of data and write each element to the flash memory
while(size--)
{
memcpy(&value, data, sizeof(uint64_t)); // alignment safe copy of byte array into 64-bit value
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, addr, value) != HAL_OK)
{
// Insert code to handle the error here
HAL_FLASH_Lock();
return;
}
addr += sizeof(uint64_t); // Advance address
data += sizeof(uint64_t); // Advance byte buffer
}
// Lock the flash memory after writing is complete
HAL_FLASH_Lock();
}
//****************************************************************************
typedef struct _FLASH_STRUCT {
uint32_t sequence;
char string[32];
uint32_t checksum;
} FLASH_STRUCT;
FLASH_STRUCT flash_struct[1] = {0};
//****************************************************************************
void test_flash(void)
{
int i;
uint8_t *p;
flash_struct->sequence++;
strcpy(flash_struct->string, "This is a test");
// Disable instruction cache prior to internal cacheable memory update
if (HAL_ICACHE_Disable() != HAL_OK)
{
Error_Handler();
}
/// Write my structure to flash
write_flash((uint8_t *)flash_struct, sizeof(flash_struct));
// Enable instruction cache after the internal cacheable memory update
if (HAL_ICACHE_Enable() != HAL_OK)
{
Error_Handler();
}
// Dump my structure in flash
p = (uint8_t *)FLASH_START_ADDRESS;
for(i=0; i<sizeof(flash_struct); i++)
{
if (i && ((i % 16) == 0)) putchar('\n');
printf(" %02X", p[i]);
}
putchar('\n');
}
//****************************************************************************
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.