2026-05-18 6:25 AM - last edited on 2026-05-18 6:31 AM by mƎALLEm
In AN2606 Rev. 70, Chap 90 Device-dependent bootloader parameters table 226
the RAM area accessible from the bootloader seem inconsistant:
- C031xx has a negative RAM range, excluding RAM at bottom and top of full RAM range as accessible from the bootloader
- C01xx RAM range declares all RAM as accessible
- C031xx excludes RAM at bottom and top of available RAM
Please confirm these values. Thanks!
2026-05-18 6:31 AM
Hello,
I didn't understand the last point:
@Uwe Bonnes wrote:
- C031xx excludes RAM at bottom and top of available RAM
2026-05-18 7:02 AM
C031 like C011 has RAM from 0x20000000 to 0x20002FFF. Table 226 tells that the range 0x20002000 up to 0x20001fff, effective nothing, is availble during bootloader. That mean that the C031 bootloader reserves all 12 k RAM for itself, while the C011 bootloader does not reserve any RAM.
2026-05-18 7:36 AM
Request raised internally over this internal ticket CDM0062723.
I'll get back to you as soon as I have a feedback.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.