2019-01-10 2:49 AM
Hello
I have build a circuit with STM32F103C8t6, and I use Keil uvision 5.11
I can upload code and " Aplicaition running" but there is " Internal command error". I test the circuit with Osiclloscope and It works
But I cannot access to watch the variable and memory the code Stop at HAL_MSPInit() and it there is error " Internal command error" again.
2019-01-10 2:55 AM
You do not tell what tool it is that generates " Internal command error".
2019-01-10 3:31 AM
I have updated thanks for reminding me
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.