2018-03-22 11:52 AM
Hi all,
So i've been banging my head up against a wall trying to work out what's been going on here...
Somehow SysTick_Handler() and so HAL_IncTick() are being optimized out (or just not included) in my Release build.
The code/project runs just fine on the target STM32F401 when complied as a Debug build.
When built as a Release build (gcc options are below), the jump location for int15 (SysTick) is the Default_Handler.
I cant understand why this is happening. The HAL libraries are unmodified, and the
HAL_IncTick() increments uwTick which is a volatile uint_32. I do use HAL_Delay(), so uwTick is referred to in the normal running of the program.
Has anyone come across this problem before?
The Release GCC options are:
arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=soft -Os -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -fno-common -ffreestanding -fsingle-precision-constant -flto -Wall -Wno-discarded-qualifiers -DSTM32F4 -DSTM32F401xC -DUSE_HAL_DRIVER -DUSE_FULL_LL_DRIVER -DHSE_VALUE=16000000 -std=gnu11 -Wbad-function-cast
GCC version is:
arm-none-eabi-gcc (GNU Tools for Arm Embedded Processors 7-2017-q4-major) 7.2.1 20170904 (release) [ARM/embedded-7-branch revision 255204]
Cube is latest version as of today, Cube F4 package version is: stm32cube_fw_f4_v1210.zip
#systick #stm322018-03-22 12:20 PM
To add to this...
Ive temporarily fixed the issue by commenting out the following lines in system_xxx.s:
.weak SysTick_Handler
.thumb_set SysTick_Handler,Default_HandlerI'm now having the same problem with the USB OTG int handler, so its not just limited to SysTick.
Any ideas?
2018-03-22 1:37 PM
Sounds more of an issue with the linker or linker script than being Cube's fault.
I'd start by looking if/why the vector table isn't being included or placed. An then the symbol attributes for the offending functions in objects they do exist in.
If C++ files or settings are being used watch out for name mangling, or explicitly use extern 'C' on the IRQ Handlers
2018-03-23 11:33 AM
Yes, you're right, it does appear to be a gcc/ld problem.
There is no C++ in this project at all, so that should not be the issue.
Using the previous version of the arm-gcc toolset fixes the problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.