2016-10-14 1:43 AM
Hi All,
I've discovered that code generated with STM32 CubeMX for SPDIFRX is faulty. SPDIFRX has dedicated PLL divider which has 2 bits (0=1/2, 1=1/4, 2=1/6 or 3=1/8), however code generates uses 4 defines which have 2, 4, 6 and 8 values. Those values are truncated to 2 bits which makes that you can select only 2 dividers:selected 1/2 (2) becomes 1/6 (2)selected 1/4 (4) becomes 1/2 (0)selected 1/6 (6) becomes 1/6 (2)selected 1/8 (8) becomes 1/2 (0)This is a $%^%$♯ frustrating because hou have to correct this after EACH code generations. I've checked this on F746 and F767 with same results!regardsMiko?aj Tutak #!stm32-!cubemx-!bug-!pll-!clock2016-10-14 3:02 AM
Hi Mikołaj Tutak,
Thank you for your feedback. The issue has been reported internally.-Syrine-2017-01-06 7:47 AM
Hi Mikołaj Tutak,
First I want to thank you for your feedback.
I check your symptoms by using CueMX 4.18 + Firmware package for F7 family version 1.5.1.
I creates new project with F746 and F767, and the field you are mentionning PeriphClkInitStruct.PLLI2S.PLLI2SP is defined as uint32.
I do not see where the cast to 2 bits is done.
Could you please elaborate a bit more, and show me where do you see it ?
Great thanks in advance for your advices.
KR
Sirma
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.