2008-08-03 11:51 AM
Bug in TIM firmware
2011-05-17 3:41 AM
Hi andreas1,
Thanks for pointing out this bug, I will escalate to our software team and let you know accordingly later on about your interesting feed-backs. Thx. Cheers, STOne-32.2011-05-17 3:41 AM
It seems there is a nasty bug in the TIM_SelectOCxM() function in FWLib v2.0.2. Apart from being horribly ugly and unreadable, the following code destroys the value of the modified CCMR register.
Code:
if((TIM_Channel == TIM_Channel_1) ||(TIM_Channel == TIM_Channel_3)) { /* Reset the OCxM bits in the CCMRx register */ *((vu32 *)((*(u32*)&TIMx) + CCMR_Offset + (TIM_Channel>>1))) &= CCMR_OC13M_Mask; /* Configure the OCxM bits in the CCMRx register */ *((vu32 *)((*(u32*)&TIMx) + CCMR_Offset + (TIM_Channel>>1))) = TIM_OCMode; } else { /* Reset the OCxM bits in the CCMRx register */ *((vu32 *)((*(u32*)&TIMx) + CCMR_Offset + ((u16)(TIM_Channel - 4)>> 1))) &= CCMR_OC24M_Mask; /* Configure the OCxM bits in the CCMRx register */ *((vu32 *)((*(u32*)&TIMx) + CCMR_Offset + ((u16)(TIM_Channel - 4)>> 1))) = (u16)(TIM_OCMode << 8); } Simply substituting '|=' for '=' should ''fix'' it, but i'd rather see it rewritten completely to something like the following.Code:
void TIM_SelectOCxM(TIM_TypeDef* TIMx, u16 TIM_Channel, u16 TIM_OCMode) { vu16* pCCMRx; u16 mask; /* Check the parameters */ assert_param(IS_TIM_123458_PERIPH(TIMx)); assert_param(IS_TIM_CHANNEL(TIM_Channel)); assert_param(IS_TIM_OCM(TIM_OCMode)); /* Disable the Channel: Reset the CCxE Bit */ TIMx->CCER &= ~(CCER_CCE_Set << TIM_Channel); if ((TIM_Channel == TIM_Channel_1) ||(TIM_Channel == TIM_Channel_3)) { mask = CCMR_OC13M_Mask; } else { mask = CCMR_OC24M_Mask; TIM_OCMode <<= 8; } if ((TIM_Channel == TIM_Channel_1) || (TIM_Channel == TIM_Channel_2)) { pCCMRx = &TIMx->CCMR1; } else { pCCMRx = &TIMx->CCMR2; } /* Configure the OCxM bits in the CCMRx register */ *pCCMRx = (*pCCMRx & mask) | TIM_OCMode; } This avoids the stupid type-punning and is probably more efficient as well. (Why is the library littered with things like taking the address of a peripheral pointer, casting it to a pointer-to-u32 and dereferencing it, often in order to compare it to a constant value? Is there any reason at all to do this, seems unnecessary to me?)We’re moving the ST Community to a new platform to give you a better and more reliable community experience.