2018-08-18 1:48 PM
When for ADC2 Channel 18 is selected as Injected Channel and initialized via “HAL_ADCEx_InjectedConfigChannel�? it will return HAL_ERROR.
When no other ADC it will fail in line 2288 2286*. When another ADC is enabled it will fail in line 2277 2275*.
HAL File: stm32h7xx_hal_adc_ex.c
HAL Version: V1.2.0 V1.3.0
I think the block from line 2229 2227* to 2290 2288* should be included in the else in line 2223 2221*.
Btw the comment in line 2245 2243* is wrong the Temp. sensor it is channel 18
It can easily reproduce by code generation of STM32CubeMX.
1. Enable ADC2 -> In18
2. Config ADC2 In18 as Injected Channel
Or use the attached CubeMX project.
*edit for Version V1.3.0
Thanks
2018-08-18 2:57 PM
>>HAL Version: V1.2.0
Not current, check if it was addressed in V1.3.0
2018-08-19 3:26 AM
Hello Clive,
tanks for the info. Unfortunately V1.3.0 it shows the same behavior.
I have edited the line numbers in the previous post to match the new version.
2018-08-19 6:12 AM
@STOne-32 @Imen DAHMEN
STM32Cube_FW_H7_V1.3.0\Drivers\STM32H7xx_HAL_Driver\Src\stm32h7xx_hal_adc.c
Quarter Battery is CH17, and not on ADC1
/* If Channel 18 is selected, enable VBAT measurement path. */
/* Note: VBAT internal internal channels available on ADC1 and ADC3 */
else if ((sConfig->Channel == ADC_CHANNEL_VBAT_DIV4) && ((hadc->Instance == ADC3)))
{
SET_BIT(tmpADC_Common->CCR, ADC_CCR_VBATEN);
}
STM32Cube_FW_H7_V1.3.0\Drivers\STM32H7xx_HAL_Driver\Src\stm32h7xx_hal_adc_ex.c
All channels wrongly commented
/* If Channel 17 is selected, enable Temp. sensor measurement path */
/* Note: Temp. sensor internal channels available only on ADC3 */
if ((sConfigInjected->InjectedChannel == ADC_CHANNEL_TEMPSENSOR) &&
(hadc->Instance == ADC3))
{
SET_BIT(tmpADC_Common->CCR, ADC_CCR_TSEN);
/* Delay for temperature sensor stabilization time */
while(WaitLoopIndex < ADC_TEMPSENSOR_DELAY_US)
{
WaitLoopIndex++;
}
}
/* If Channel 18 is selected, enable VBAT measurement path */
/* Note: VBAT internal internal channels available only on ADC3 */
else if ((sConfigInjected->InjectedChannel == ADC_CHANNEL_VBAT_DIV4) &&
(hadc->Instance == ADC3))
{
SET_BIT(tmpADC_Common->CCR, ADC_CCR_VBATEN);
}
/* If Channel 0 is selected, enable VREFINT measurement path */
/* Note: VREFINT internal channels available only on ADC3 */
else if ((sConfigInjected->InjectedChannel == ADC_CHANNEL_VREFINT) &&
(hadc->Instance == ADC3))
{
SET_BIT(tmpADC_Common->CCR, ADC_CCR_VREFEN);
}
else
{
/* Discrepancy found out between ADC instance and internal
channel request */
SET_BIT(hadc->State, HAL_ADC_STATE_ERROR_CONFIG);
tmp_hal_status = HAL_ERROR;
}
The error reported above occurs because the top level test doesn't qualify for ADC3 and it causes a drop through to a HAL_ERROR
/* If the requested internal measurement path has already been enabled, */
/* bypass the configuration processing. */
if (( (sConfigInjected->InjectedChannel == ADC_CHANNEL_TEMPSENSOR) &&
(HAL_IS_BIT_CLR(tmpADC_Common->CCR, ADC_CCR_TSEN)) ) ||
( (sConfigInjected->InjectedChannel == ADC_CHANNEL_VBAT_DIV4) &&
(HAL_IS_BIT_CLR(tmpADC_Common->CCR, ADC_CCR_VBATEN)) ) ||
( (sConfigInjected->InjectedChannel == ADC_CHANNEL_VREFINT) &&
(HAL_IS_BIT_CLR(tmpADC_Common->CCR, ADC_CCR_VREFEN)))
)
{
2018-08-19 6:12 AM
/* If the requested internal measurement path has already been enabled, */
/* bypass the configuration processing. */
if (( (sConfigInjected->InjectedChannel == ADC_CHANNEL_TEMPSENSOR) &&
(HAL_IS_BIT_CLR(tmpADC_Common->CCR, ADC_CCR_TSEN)) ) ||
( (sConfigInjected->InjectedChannel == ADC_CHANNEL_VBAT_DIV4) &&
(HAL_IS_BIT_CLR(tmpADC_Common->CCR, ADC_CCR_VBATEN)) ) ||
( (sConfigInjected->InjectedChannel == ADC_CHANNEL_VREFINT) &&
(HAL_IS_BIT_CLR(tmpADC_Common->CCR, ADC_CCR_VREFEN)))
)
{
/* Configuration of common ADC parameters (continuation) */
/* Software is allowed to change common parameters only when all ADCs */
/* of the common group are disabled. */
if ((ADC_IS_ENABLE(hadc) == RESET) &&
(ADC_ANY_OTHER_ENABLED(hadc) == RESET) )
{
/* If Channel 17 is selected, enable Temp. sensor measurement path */
/* Note: Temp. sensor internal channels available only on ADC3 */
if ((sConfigInjected->InjectedChannel == ADC_CHANNEL_TEMPSENSOR) &&
(hadc->Instance == ADC3))
{
SET_BIT(tmpADC_Common->CCR, ADC_CCR_TSEN);
/* Delay for temperature sensor stabilization time */
while(WaitLoopIndex < ADC_TEMPSENSOR_DELAY_US)
{
WaitLoopIndex++;
}
}
/* If Channel 18 is selected, enable VBAT measurement path */
/* Note: VBAT internal internal channels available only on ADC3 */
else if ((sConfigInjected->InjectedChannel == ADC_CHANNEL_VBAT_DIV4) &&
(hadc->Instance == ADC3))
{
SET_BIT(tmpADC_Common->CCR, ADC_CCR_VBATEN);
}
/* If Channel 0 is selected, enable VREFINT measurement path */
/* Note: VREFINT internal channels available only on ADC3 */
else if ((sConfigInjected->InjectedChannel == ADC_CHANNEL_VREFINT) &&
(hadc->Instance == ADC3))
{
SET_BIT(tmpADC_Common->CCR, ADC_CCR_VREFEN);
}
else
{
/* Discrepancy found out between ADC instance and internal
channel request */
SET_BIT(hadc->State, HAL_ADC_STATE_ERROR_CONFIG);
tmp_hal_status = HAL_ERROR;
}
}
/* If the requested internal measurement path has already been enabled */
/* and other ADC of the common group are enabled, internal */
/* measurement paths cannot be enabled. */
else
{
/* Update ADC state machine to error */
SET_BIT(hadc->State, HAL_ADC_STATE_ERROR_CONFIG);
tmp_hal_status = HAL_ERROR;
}
}
2018-08-19 6:20 AM
@Kilian Nötzold definitely a complete mess, flagged to staff.
/* Configuration of common ADC parameters */
if((hadc->Instance == ADC1) || (hadc->Instance == ADC2))
{
/* Pointer to the common control register */
tmpADC_Common = ADC12_COMMON_REGISTER(hadc);
}
else
{
/* Pointer to the common control register */
tmpADC_Common = ADC3_COMMON_REGISTER(hadc);
} // MOVE THIS BRACE OVER/AROUND THE OFFENDING CODE FOR ADC3 BELOW
2018-08-19 10:56 AM
@Community member Thanks for informing ST.
Whoever is taking care on this topic should also check if a similar issue exists in stm32h7xx_hal_adc.c staring in line 2548 as the code looks Identical. I haven’t looked deeper into but at least the comments are messed in the same way.
2019-01-18 5:16 PM
FYI The same issue exists for stm32h7xx_hal_adc.c
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.