2011-08-23 12:09 PM
I have a project with STM32F107.
I have a custom bootloader at address 0x08000000 and an application at the address 0x0809000. I can perfectly program an application from a bootloader, and an application works fine after that (vector table is relocated to the application address). Nevertheless when I am trying to program a bootloader from an application, it hangs at erasing pages. Pages are not protected. And I am using exactly the same functions (with different addresses) that I am using for programming from the bootloader. Please, if someone has a clue on what it could be, point me in a right direction. Gennady2011-08-25 2:09 AM
I think you had enable the RDP.
And the first 4KB of flash will be write-protected default when RDP is enabled. You should change the BootLoader to start from 0x08001000, to skip the first 4KB. And put a tiny bootloader at 0x08000000~0x08000fff, to jump to your bootloader. Cheers! James Peng www.mcuisp.com World's first! Versatile Handy Programmer, EP968, STM32 STM8 supportted!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.