2019-11-22 2:42 AM
Hi,
i have STM32H7 Nucleo board, i'm trying to implement CAN-FD. so i was trying to send some data over CAN-FD to CAN-Analyser. For bit timing calculation i'm using STM32H743I-EVAL example as reference .
fdcan_ker_ck - 20Mhz, Time_quantum- 50ns, Propagation_segment- 23 tq, Phase_segment_1- 8 tq, Phase_segment_2- 8 tq, Synchronization_Jump_width - 8 tq, Bit_length - 2 us, Bit_rate- 0.5 MBit/s.
this i used it for both nominal and data..But when i use it can analyser the bit timing doesn't match.i used these following documents for reference but still couldn't solve it
https://www.can-cia.org/fileadmin/resources/documents/proceedings/2013_hartwich_v2.pdf
Thanks,
Vimal
2019-11-24 10:33 PM
Hi,
I'm getting some data in analyser but couldn't able to decode the data, this is because of bit timing issue or anything else. i'm attaching the screenshot, please have a look into it.
Auto-retransmission is happening because my Nucleo-board is not getting any acknowledgement
Thanks,
Vimal
2019-11-29 2:20 AM
Hi,
Issue solved, there is issue with the crystal oscillator.Now it works fine with internal oscillator.
thanks,
Vimal
2021-03-08 7:49 AM
Hi VPras,
I am also facing the same issue. Bit timings are not matching when i see it in the oscilloscope. I am using NUCLEO-H743ZI board provided by ST partner.
Should i change the crystal oscillator on the board? Board is provided by ST partner, then how can this be the issue of the crystal oscillator?
Any help would be highly appreciated.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.