2016-11-14 8:56 PM
Hi!
I have LAN8720, STM32F4DISCOVERY, CP2102I connected PC-LAN8720, LAN8720-STM32F4DISC, STM32F4DISC-CP2102, CP2102-PC.I wrote such program for STM32F407://Ethernet/*******************************************************************///pc6-usart6_tx,pc7-usart6_rx//pb13-tx1, pb11-txen, pb12-tx0, pc4-rx0, pc5-rx1, pa1-refclk, pa7-crs, pa2-mdio,pc1-mdc#include ''stm32f4xx.h''uint32_t i, temp;int main(){//config clockRCC->CR=(RCC_CR_HSEON|RCC_CR_PLLON|RCC_CR_CSSON);//extern quartz,pll,(|RCC->PLLCFGR=0x00005408;//n=210, m=10, hs=8 MHz//RCC->CFGR=(RCC_CFGR_SW_PLL|RCC_CFGR_SWS_PLL|RCC_CFGR_MCO1);//mco1,system clock from PLLRCC->CFGR=0x0760940A;while (!(RCC->CR&0x02000000));//enable gpio, usart6, macRCC->AHB1ENR=(RCC_AHB1ENR_ETHMACRXEN|RCC_AHB1ENR_ETHMACTXEN|RCC_AHB1ENR_ETHMACEN|RCC_AHB1ENR_GPIOAEN|RCC_AHB1ENR_GPIOBEN|RCC_AHB1ENR_GPIOCEN|RCC_AHB1ENR_GPIODEN);//vkl takt port a-d,macRCC->APB2ENR=(RCC_APB2ENR_SYSCFGEN|RCC_APB2ENR_USART6EN);//config type GPIOGPIOA->MODER|=(GPIO_MODER_MODER1_1|GPIO_MODER_MODER2_1|GPIO_MODER_MODER7_1|GPIO_MODER_MODER8_1);GPIOB->MODER|=(GPIO_MODER_MODER12_1|GPIO_MODER_MODER13_1|GPIO_MODER_MODER15_1);GPIOC->MODER=(GPIO_MODER_MODER1_1|GPIO_MODER_MODER4_1|GPIO_MODER_MODER5_1|GPIO_MODER_MODER6_1|GPIO_MODER_MODER7_1);GPIOD->MODER=0x55000000;//VIVODI PD15-PD12 - VIHOD//config altern func GPIOA->AFR[0]=0xB0000BB0;//mac GPIOB->AFR[1]=0xB0BB0000;//mac GPIOC->AFR[0]=0x88BB00B0;//PC6,PC7-USART6,mac//conf usart6 //USART6->BRR=0x0341;//0x0341,8 MHz to 9600 bps USART6->BRR=0x8b;//8 MHz to 115200 bps USART6->CR1|=(USART_CR1_OVER8|USART_CR1_RE|USART_CR1_TE|USART_CR1_UE);//over8=1,UE,TE,RE//set rmii interfaceSYSCFG->PMC=SYSCFG_PMC_MII_RMII_SEL;//config LAN8720ETH->MACMIIDR=0x00001000;//auto-negotiationETH->MACMIIAR=0x00000803;//adr=1, reg=0,write while (ETH->MACMIIAR==0x00000803);for (i=0;i<10;i++);while (1){ETH->MACMIIAR=0x00000841;//adr=1, reg=1,readwhile (ETH->MACMIIAR==0x00000841);while (!(ETH->MACMIIDR&0x0004))//link is up?{//no ETH->MACMIIAR=0x00000841;//adr=1, reg=1,read while (ETH->MACMIIAR==0x00000841); GPIOD->ODR=0x00004000;}GPIOD->ODR=0x00001000;//yesfor (i=0;i<10000;i++);GPIOD->ODR=0x00000000;//yes//out reg 1temp=ETH->MACMIIDR;USART6->DR=temp;while (!(USART6->SR&USART_SR_TXE));temp=temp>>8;USART6->DR=temp;while (!(USART6->SR&USART_SR_TXE));ETH->MACMIIAR=0x00000fc1;//adr=1, reg=31,readwhile (ETH->MACMIIAR==0x00000fc1);//out reg31temp=ETH->MACMIIDR;USART6->DR=temp;while (!(USART6->SR&USART_SR_TXE));temp=temp>>8;USART6->DR=temp;while (!(USART6->SR&USART_SR_TXE));//config MACETH->MACCR=0x02008080;//crsc strip, pad/crc stripswitch(ETH->MACMIIDR){ case 0x1044:ETH->MACCR|=0x00008000;//10,h break; case 0x1054:ETH->MACCR|=0x00008800;//10,f break; case 0x1048:ETH->MACCR|=0x0000c000;//100,h break; case 0x1058:ETH->MACCR|=0x0000c800;//100,f break; default: GPIOD->ODR=0x00004000; while (1); break;}ETH->MACCR|=0x00000004;//reGPIOD->ODR=0x00001000;//out MACCRtemp=ETH->MACCR;USART6->DR=temp;while (!(USART6->SR&USART_SR_TXE));temp=temp>>8;USART6->DR=temp;while (!(USART6->SR&USART_SR_TXE));temp=temp>>8;USART6->DR=temp;while (!(USART6->SR&USART_SR_TXE));temp=temp>>8;USART6->DR=temp;while (!(USART6->SR&USART_SR_TXE));while (!(ETH->MACDBGR&0x00000010)){ GPIOD->ODR=0x00008000;//yes}GPIOD->ODR=0x00001000;//yeswhile (1);//out MACDBGRtemp=ETH->MACDBGR;USART6->DR=temp;while (!(USART6->SR&USART_SR_TXE));temp=temp>>8;USART6->DR=temp;while (!(USART6->SR&USART_SR_TXE));temp=temp>>8;USART6->DR=temp;while (!(USART6->SR&USART_SR_TXE));temp=temp>>8;USART6->DR=temp;while (!(USART6->SR&USART_SR_TXE));}}There are right impulses on pins rx0, rx1, refclk, crs on LAN8720.In docklight I saw 2d 78 58 10 84 C8 00 02. (Link is up in LAN8720, speed and mode of ethernet are defined).Why is bit RFWRA in register MACDBGR not set? What is wrong?Thank You!2016-11-14 9:12 PM
Bytes in docklight are in hex format!
2016-11-15 12:48 AM
I don't say this is the reason of failure for sure, but mind that we are talking 50MHz here, and signal consistency is not trivial anymore. I had troubles to get RMII working on the STM3240G-EVAL board, because of the refclk track was some 15cm long; I succeeded with cutting the trace and routing it with a cca 10cm wire...
So the question is, what is the source of the 50MHz reference clock and how is that and other Rx signals exactly routed. You might perhaps want to start with with a known working board, maybe some of the Nucleo144 offerings. JW2016-11-15 1:24 AM
The refclk goes from LAN8720 and LAN8720 connected to STM32F407 through 11 single wires. The length of each wire is about 15 cm.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.