2023-03-08 6:21 AM
Hi,
I am playing around with Timers on Nucleo-G031 at 64MHz clocked from HSI and PLL.
I use TIM1 with AutoReload of 6 and Capture/Compare Value of 3 to create an 9.17MHz 50% duty-cycle signal.
The signals turns out to have 46.4ns high-pulse and 62.8ns low-pulse, which is quite assymetric
Any ideas where this comes from, and what to do as a remedy?
Can this be caused by using internal resonator? Or to ask the other way round: will an external crystal yield better results?
2023-03-08 6:34 AM
That is perfectly fine with your settings:
9.17 MHz = 64 MHz / (ARR + 1)
and with an odd maximum of ARR + 1 (because CNT = 0 is a valid value) you will never get 50% duty cycle.
So change ARR to an odd value.
HSI itself is not so accurate, depending on the application it might be too jittery.
2023-03-08 6:36 AM
ARR value of 6 yields the period of 7 cycles and CCR value of 3 gives 3/7 duty. STM32G series TIM1 may be clocked at 128 MHz - try to use this feature.
2023-03-08 9:44 PM
Ohhh... ********...
Thank you for pointing this out to me!
I studied the datasheet a bit further and found that the center-aligned mode might as well suit the need for a symetrical, 50% duty-cycle signal.
Will definetly try the 128MHz clock, this might be helpful for another problem!
Thanks!
2023-03-08 10:23 PM
You don't need center-aligned mode for 50% duty cycle PWM. Use odd ARR values, or use the Toggle mode instead of PWM.
JW
2023-03-08 10:25 PM
and yet more possibilities, thanks!
May I ask why you don't recommend center-aligned mode?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.