2021-11-15 5:59 PM
I used the sram and got a 0.37 , Pretty sure this is not right.
I use -O2 and hard-float, others remain default.
Can any one tell me what should I do next?
2021-11-15 7:27 PM
I don't spend a lot of time dwelling on this, but an M4F should probably yield closer to a 0.7 if the code and libraries are optimized.
One of the issues here is that this one doesn't have ITCM//DTCM RAM to work with, or a FLASH/ART path into the prefetcher.
Which SRAM are you using? SRAM[1..3] would be the closest coupled.
2021-11-16 12:19 AM
I use the SRAM1, which starts from 0x10000000. According official document, the score should be 1.25. Still a long gap.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.