2022-03-08 8:51 AM
2022-03-08 9:18 AM
Do a diff on the code between the two and see what's different.
2022-03-08 9:43 AM
There is no difference, it's the same code.
File ioc was migrated from 6.4 to 6.5
IDE 1.8
HAL 1.16.2
Toolchain 9-2020-q2
IDE 1.9
HAL 1.16.2
Toolchain 10.3-2021.10
2022-03-08 9:57 AM
2022-03-08 12:41 PM
V. 1.9 uses a newer toolchain by default (compiler GCC 10).
2022-03-08 1:18 PM
using ide 1.9 and Toolchain 9-2020-q2
works well.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.