2011-12-23 3:09 AM
Hello,
i am programming the bootloader for the stm32f103c8 mcu. The SW has bootloader part and application part. In the application I use the function NVIC_GenerateSystemReset() to reset the mcu to the bootloader mode. In the debug mode( the Jlink ist connected to the board), the bootloader works well, the user code can be downloaded to the mcu over the can bus. but If I dont use the debugger. the SW collapse after the function NVIC_GenerateSystemReset() is called. The user code can not be downloaded. The interrupt vector address I used is following bootloader :0x0800 0000 Application: 0x0800 4000 I have investigated in this problem for a week long and can not solve this problem. Can somebody help me, it is driving me crazy! best Regards Chunyu2011-12-23 7:04 AM
It should work in a reasonably predictable way, if you are using the V2 library, I would generally recommend a ''while(1);'' after the call.
The code in the reset path might provide some insight. I'd be tempted to add some assembler code to send some data to a serial port very early to confirm it is getting there. I'd look very carefully at the initial conditions, and how various peripherals are being set up, the JTAG debugger isn't totally transparent in this regard. From a hardware perspective, the system won't reset properly is you have external circuitry driving NRST high, also consider the state of the BOOTx pins. This assembler should also be viable to reset the CPUSystemReset PROC
EXPORT SystemReset
ldr r1, =0xE000ED0C ; NVIC Application Interrupt and Controller
ldr r0, =0x05FA0004 ; Magic
str r0, [r1, #0] ; Reset
b .
bx lr
ENDP
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.