2024-09-16 4:57 AM - edited 2024-10-01 12:08 AM
Hello.
I have problems to get DMA with ADC working.
I'd like to collect 2 values from PA3 and PA4 and store them in an array (convertedData_u16). I configured ADC1 with Channels 8 and 9, and GPDMA1 with Channel1.
I can see that data is being collected in ADC1->DR (cannot validate if they are plausible at the moment).
What I also see is that the clocks for GPIOA, ADC1 and GPDMA1 are enabled (RCC_AHB1ENR->GPDMA1EN = 1; RCC_AHB2ENR1->GPIOAEN = 1; RCC_AHB2ENR1->ADC12EN = 1) and ADC1 (ADC1_CR->ADEN = 1) and GPDMA1 Channel1 (GPDMA_C1CR->EN = 1) are enabled.
However, I have not achieved to get data into convertedData_u16.
What is wrong with my code? What else can I do to find the error?
#include "main.h"
#define DMA_PERIPHERAL GPDMA1
#define DMA_CHANNEL LL_DMA_CHANNEL_1
#define ADC_PERIPHERAL ADC1
#define ADC_CHANNEL_COUNT 2
#define ADC_CONVERTED_DATA_BUFFER_SIZE ((uint32_t) 32) /* Size of array aADCxConvertedData[] */
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma1;
static uint16_t convertedData_u16[ADC_CHANNEL_COUNT];
void SystemClock_Config(void);
void ADC1_IRQHandler(void);
void GPDMA1_Channel1_IRQHandler(void);
void InitADC_V();
void InitDMA_V(void);
void ConfigurePorts_V();
int main(void)
{
HAL_Init();
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWREx_EnableVddA();
SystemClock_Config();
ConfigurePorts_V();
InitADC_V();
InitDMA_V();
LL_ADC_EnableIT_EOS(ADC_PERIPHERAL); // End of sequence flag
while (1)
{
HAL_ADC_Start_DMA(&hadc1, (uint32_t *)convertedData_u16,
(ADC_CONVERTED_DATA_BUFFER_SIZE));
HAL_Delay(1000);
}
}
void Error_Handler(void)
{
__disable_irq();
while (1)
{
}
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_MSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.MSIState = RCC_MSI_ON;
RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_4;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;
RCC_OscInitStruct.PLL.PLLMBOOST = RCC_PLLMBOOST_DIV1;
RCC_OscInitStruct.PLL.PLLM = 1;
RCC_OscInitStruct.PLL.PLLN = 80;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLLVCIRANGE_0;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_PCLK3;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
{
Error_Handler();
}
}
void ConfigurePorts_V(void)
{
__HAL_RCC_GPIOA_CLK_ENABLE();
GPIO_InitTypeDef GPIO_InitStruct = { 0 };
GPIO_InitStruct.Pin = GPIO_PIN_3 | GPIO_PIN_4;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
}
void InitDMA_V(void)
{
__HAL_RCC_GPDMA1_CLK_ENABLE();
hdma1.Instance = GPDMA1_Channel1;
hdma1.Init.Request = GPDMA1_REQUEST_ADC1;
hdma1.Init.BlkHWRequest = DMA_BREQ_BLOCK;
hdma1.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma1.Init.SrcInc = DMA_SINC_FIXED;
hdma1.Init.DestInc = DMA_DINC_INCREMENTED;
hdma1.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_WORD;
hdma1.Init.DestDataWidth = DMA_DEST_DATAWIDTH_WORD;
hdma1.Init.Priority = DMA_LOW_PRIORITY_LOW_WEIGHT;
hdma1.Init.SrcBurstLength = 1;
hdma1.Init.DestBurstLength = 1;
hdma1.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT0|DMA_DEST_ALLOCATED_PORT0;
hdma1.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
hdma1.Init.Mode = DMA_NORMAL;
HAL_DMA_Init(&hdma1);
__HAL_LINKDMA(&hadc1, DMA_Handle, hdma1);
NVIC_SetPriority(GPDMA1_Channel1_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),0, 0));
NVIC_EnableIRQ(GPDMA1_Channel1_IRQn);
}
void InitADC_V(void)
{
ADC_ChannelConfTypeDef sConfig = {0};
// LL_RCC_SetADCDACClockSource(LL_RCC_ADCDAC_CLKSOURCE_HSI);
__HAL_RCC_ADC1_CLK_ENABLE();
hadc1.Instance = ADC_PERIPHERAL;
hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV128;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.GainCompensation = 0;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc1.Init.LowPowerAutoWait = DISABLE;
hadc1.Init.ContinuousConvMode = DISABLE;
hadc1.Init.NbrOfConversion = 2;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.DMAContinuousRequests = ENABLE;
hadc1.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hadc1.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR;
hadc1.Init.OversamplingMode = DISABLE;
HAL_ADC_Init(&hadc1);
sConfig.Channel = ADC_CHANNEL_9;
sConfig.Rank = ADC_REGULAR_RANK_2;
sConfig.SamplingTime = ADC_SAMPLETIME_5CYCLE;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
sConfig.Channel = ADC_CHANNEL_8;
sConfig.Rank = ADC_REGULAR_RANK_1;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
LL_ADC_EnableIT_EOS(ADC_PERIPHERAL);
LL_ADC_StartCalibration(ADC_PERIPHERAL, LL_ADC_SINGLE_ENDED);
HAL_Delay(50);
NVIC_SetPriority(ADC1_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(), 0, 0));
NVIC_EnableIRQ(ADC1_IRQn);
}
void GPDMA1_Channel1_IRQHandler(void)
{
if (LL_DMA_IsActiveFlag_TC(DMA_PERIPHERAL, DMA_CHANNEL) == 1)
{
LL_DMA_ClearFlag_TC(DMA_PERIPHERAL, DMA_CHANNEL);
}
}
void ADC1_IRQHandler(void)
{
if (LL_ADC_IsActiveFlag_EOS(ADC_PERIPHERAL))
{
LL_ADC_ClearFlag_EOS(ADC_PERIPHERAL);
}
else if (LL_ADC_IsActiveFlag_EOC(ADC_PERIPHERAL))
{
LL_ADC_ClearFlag_EOC(ADC_PERIPHERAL);
}
else if (LL_ADC_IsActiveFlag_OVR(ADC_PERIPHERAL) != 0)
{
LL_ADC_ClearFlag_OVR(ADC_PERIPHERAL);
}
else if (LL_ADC_IsActiveFlag_EOSMP(ADC_PERIPHERAL) != 0) // Ist nicht aktiviert
{
LL_ADC_ClearFlag_EOSMP(ADC_PERIPHERAL);
}
}
2024-10-08 2:30 AM
No one here who can help me?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.