2019-09-24 7:33 AM
i would like to switch the LED ON (PB0) when ADC is from above threshold value ''if (adcValue >2275)''
and in case of below threshold it should switch LED ON (PB1)
code showing no error in Keil , if you see any erroe plz highlight me thanks.
//************************************** ADC simple software trigger
#include <stdio.h>
#include "stm32f10x.h" // Device header
#include "stm32f10x_adc.h" // Keil::Device:StdPeriph Drivers:ADC
#include "stm32f10x_rcc.h" // Keil::Device:StdPeriph Drivers:RCC
#include "stm32f10x_gpio.h" // Keil::Device:StdPeriph Drivers:GPIO
GPIO_InitTypeDef GPIO_InitStructure;
ADC_InitTypeDef ADC_InitStructure;
int main ()
{
uint16_t adcValue;
//----------------------------------------------------------------------------------------
// ******************************ADC ******************************
//----------------------------------------------------------------------------------------
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB, ENABLE);
//RCC_ADCCLKConfig(RCC_PCLK2_Div6); //clock for ADC (max 14MHz --> 72/6=12MHz) APB2 operates at full speed 72 MHz
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; //Analog signal Input
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;
GPIO_Init(GPIOA, &GPIO_InitStructure);
// TWO LEDS that will blink when voltage is raised to above threshold
GPIO_InitStructure.GPIO_Pin =GPIO_Pin_0| GPIO_Pin_1;
GPIO_InitStructure.GPIO_Mode =GPIO_Mode_Out_PP;
GPIO_InitStructure.GPIO_Speed= GPIO_Speed_50MHz;
GPIO_Init(GPIOB, &GPIO_InitStructure);
ADC_InitStructure.ADC_Mode =ADC_Mode_Independent; //one ADC used, other is dual mode.
ADC_InitStructure.ADC_ScanConvMode = DISABLE; //ONLY single channel conversion is used.
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; //the ADC starts another conversion as soon as it finishes one.
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfChannel=1;
ADC_InitStructure.ADC_ExternalTrigConv= DISABLE;
ADC_InitStructure.ADC_ExternalTrigConv= ADC_ExternalTrigConv_None;
ADC_Init(ADC1, &ADC_InitStructure); //init ADC
// Select input channel for ADC1
// ADC1 channel 0 (PA0)
ADC_RegularChannelConfig(ADC1, ADC_Channel_0, 1, ADC_SampleTime_13Cycles5);
// Start ADC conversion
ADC_SoftwareStartConvCmd(ADC1, ENABLE);
// Wait until ADC conversion finished
while (!ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC))
{
adcValue= ADC_GetConversionValue(ADC1);
}
if (adcValue >2275)
{
GPIOB->BSRR = GPIO_BSRR_BS0; // set GPIOB.0
}
if (adcValue < 2275)
{
GPIOB->BSRR = GPIO_BSRR_BS1; // set GPIOB.1
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.