2015-05-16 9:34 AM
I have a project with 3 channels DMA with STM32F407VGT (STM32F4-Discovery). The channels 2,3 and 4 (PA2, PA3, PA4) are used to read the ADC values. Its enough to read the values every 10 seconds. So the poling mode is also good enough. I tried Regolar poling, regular with Interrup, injected polling,.... but have always the same problem. The ADC/DMA ready only the first channel and not second or third channel. with below config, DMA and 3 regular Channels which is produced by MxCube.
&sharpinclude ''adc.h''&sharpinclude ''gpio.h''&sharpinclude ''dma.h''ADC_HandleTypeDef hadc1;DMA_HandleTypeDef hdma_adc1;void MX_ADC1_Init(void){ ADC_ChannelConfTypeDef sConfig; hadc1.Instance = ADC1; hadc1.Init.ClockPrescaler = ADC_CLOCKPRESCALER_PCLK_DIV8; hadc1.Init.Resolution = ADC_RESOLUTION12b; hadc1.Init.ScanConvMode = DISABLE; hadc1.Init.ContinuousConvMode = DISABLE; hadc1.Init.DiscontinuousConvMode = DISABLE; hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc1.Init.NbrOfConversion = 3; hadc1.Init.DMAContinuousRequests = ENABLE; hadc1.Init.EOCSelection = EOC_SINGLE_CONV; HAL_ADC_Init(&hadc1); sConfig.Channel = ADC_CHANNEL_2; sConfig.Rank = 1; sConfig.SamplingTime = ADC_SAMPLETIME_480CYCLES; HAL_ADC_ConfigChannel(&hadc1, &sConfig); sConfig.Channel = ADC_CHANNEL_3; sConfig.Rank = 2; HAL_ADC_ConfigChannel(&hadc1, &sConfig); sConfig.Channel = ADC_CHANNEL_4; sConfig.Rank = 3; HAL_ADC_ConfigChannel(&hadc1, &sConfig);}void HAL_ADC_MspInit(ADC_HandleTypeDef* hadc){ GPIO_InitTypeDef GPIO_InitStruct; if(hadc->Instance==ADC1) { __ADC1_CLK_ENABLE(); GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_4; GPIO_InitStruct.Mode = GPIO_MODE_ANALOG; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); hdma_adc1.Instance = DMA2_Stream0; hdma_adc1.Init.Channel = DMA_CHANNEL_0; hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY; hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE; hdma_adc1.Init.MemInc = DMA_MINC_ENABLE; hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD; hdma_adc1.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD; hdma_adc1.Init.Mode = DMA_NORMAL; hdma_adc1.Init.Priority = DMA_PRIORITY_MEDIUM; hdma_adc1.Init.FIFOMode = DMA_FIFOMODE_DISABLE; HAL_DMA_Init(&hdma_adc1); __HAL_LINKDMA(hadc,DMA_Handle,hdma_adc1); }}void main(){ uint16_t ADValues[3]; HAL_ADC_MspInit(); MX_DMA_Init(); MX_ADC1_Init(); HAL_ADC_Start_DMA(&hadc1, (uint32_t *)&ADValues[0], 3);}Wahts is the problem? Can somebody help me?Thanls a lot in advance for your help.Osto #adc2015-05-16 9:41 AM
hadc1.Init.ScanConvMode = DISABLE;
// << Probably want it to be scanning the channels?2015-05-16 11:08 AM
It's Discovery deja vu all over again.
PA4 is also connected to the board audio codec's LRCK pin. Suggest changing to ADC channels 1, 2 and 3. Cheers, Hal2015-05-16 2:53 PM
Thanks clive. That was the problem.
2015-05-16 2:54 PM
Yes, I know that PA4 pin is in use.
I removed the chip from the board.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.