2024-06-25 1:34 PM
Hallo Gurus:
Newbie level question..'health issues' making me less efficient, and some pointers to get me started would help a lot.
I want to do a software start of ADC conversions with DMA into a circular buffer...when an external trigger (GPIO?) occurs, start a timer, and have timer compare stop the conversion...like an oscilloscope triggered capture with pre- and post-trigger capture?
Just pointers into the "RTFM", or app note/tutorial, if possible, not wanting to dump a design exercise on anyone!
Solved! Go to Solution.
2024-06-25 1:50 PM - edited 2024-06-25 2:04 PM
This could be a starting point: STM32 CubeMX “Timer + ADC + DMA” – Bart Slinger
The timer could be started by a EXTI interrupt from the EXtI IRQ handler (software) or even by using ETR (external trigger) in the timer
hth
KnarfB
2024-06-25 1:50 PM - edited 2024-06-25 2:04 PM
This could be a starting point: STM32 CubeMX “Timer + ADC + DMA” – Bart Slinger
The timer could be started by a EXTI interrupt from the EXtI IRQ handler (software) or even by using ETR (external trigger) in the timer
hth
KnarfB
2024-06-25 2:03 PM
Hello der Knarf! Danke, merçi, obrigado, thanks, shukran...(Trying to be "inclusive":smiling_face_with_halo:)
I'll have a look at this tomorrow (CEST here...) and will mark as solution, if my tired old brain can get around it 🥵
Just the kind of thing I'm looking for!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.