2020-01-30 7:50 AM
Hi,
I have a Problem with the NUCLEO-L476RG.
I tried to activate USART2.
Sending a single Char to a Terminal Programm like Putty or HTERM.
I took the guide from the reference Manual on Page 1341.
But it wont work.
#include "stm32l4xx.h"
#include "stm32l4xx_nucleo.h"
int main(void)
{
//MSI CLK setup
RCC->CR |=RCC_CR_MSIRGSEL;// enable the MSI CLK
RCC->CR &= RCC_CR_MSIRANGE_0;
// deleting the reset value
RCC->CR |= RCC_CR_MSIRANGE_11;
// setting MSI CLK to 48MHz
// USART Setting
RCC->AHB2ENR |= RCC_AHB2ENR_GPIOAEN;
GPIOA->MODER &= ~GPIO_MODER_MODER2_1;
//alternetive mode for PA2
GPIOA->AFR[0] |= 0b0111 << GPIO_AFRL_AFSEL2_Pos;
//alternetive function 7 for PA2
RCC->APB1ENR1 |= RCC_APB1ENR1_USART2EN;
//enable clock for Usart2
//Guide on Page 1341
USART2->CR1 |= USART_CR1_M;
// setting the word length
USART2->BRR = 417;
// setting 115200 Baud
//=> 48e6/115200=416,666666
// Stop Bit Programming not necessary,
//reset value -> 1 Stop Bit
// DMA not necessary , or isn't it ?
USART2->CR1 |= USART_CR1_UE|USART_CR1_TE;
// USART2 Enable , Transmitter Enable
char c = 'C';
for(;;){
volatile unsigned int i =4800000;
while(i--);
while (
(USART2->ISR & USART_ISR_TXE) == 0);
USART2->TDR=c;
}
}Have i forgotten something or done anything wrong?
Thanks,
Dominik
2020-01-30 8:58 AM
Honestly, if you choose to program at the register level, you really need to learn how to debug at that level also.
If the debugger has a "Peripheral View" use that to descend into the register nodes and check them against expectations set by the Data Sheet and Reference Manual.
Pretty sure you can't arbitrarily change the clock you're currently running from.
2020-01-30 10:33 AM
> Pretty sure you can't arbitrarily change the clock you're currently running from.
Namely you can't switch to high clock without changing FLASH latency (and in some families, maybe not in 'L4, internal LDO regulator setting).
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.