2015-10-29 2:56 AM
Hi,my friend,
I want to implement the both TX/RX channel of SAI, but can not find any code sample in STM32CUBE. I want to use DMA to transfer audio data between SAI and codec and start the TX/RX DMA at once and just use one DMA interrupt callback to process data. Now I can run the SAI_AudioPlay sample to play audio file on my board and which just use the SAI1B, working in slave mode. I add some code to init the SAI1A as the SAI1B, but found no data recieved in the RX buffer, but TX is work fine. Any one could help me ? Many thanks! #sai-stm32f7We’re moving the ST Community to a new platform to give you a better and more reliable community experience.