2021-03-03 9:59 PM
Hi,
It may seem simple to you, but it confuses me for a bit of time after I saw:
uint32_t isrflags = READ_REG(huart->Instance->SR);
and
#define READ_REG(REG) ((REG))
I have 2 questions here:
huart->Instance->SR should be an address, how does READ_REG(REG) get the data from it without using like:
#define READ_REG(REG) (*(REG))
Why there are double layers of parentheses for REG as ((REG))? I searched but seems get nothing.
Thanks so much for your time!
Regards,
2021-03-04 1:13 AM
Where did you find these defines?
2021-03-04 5:06 PM
Hi Uwe,
I found this function in stm32f4xx_hal_uart.c:
/**
* @brief This function handles UART interrupt request.
* @param huart Pointer to a UART_HandleTypeDef structure that contains
* the configuration information for the specified UART module.
* @retval None
*/
void HAL_UART_IRQHandler(UART_HandleTypeDef *huart)
{
uint32_t isrflags = READ_REG(huart->Instance->SR);
uint32_t cr1its = READ_REG(huart->Instance->CR1);
uint32_t cr3its = READ_REG(huart->Instance->CR3);
uint32_t errorflags = 0x00U;
uint32_t dmarequest = 0x00U;
/* If no error occurs */
errorflags = (isrflags & (uint32_t)(USART_SR_PE | USART_SR_FE | USART_SR_ORE | USART_SR_NE));
if (errorflags == RESET)
{
/* UART in mode Receiver -------------------------------------------------*/
if (((isrflags & USART_SR_RXNE) != RESET) && ((cr1its & USART_CR1_RXNEIE) != RESET))
{
UART_Receive_IT(huart);
return;
}
}
……
Then in stm32f4xx.h, near bottom:
#define READ_REG(REG) ((REG))
Thanks!
Regards,
2023-12-13 12:14 PM
>> huart->Instance->SR should be an address, how does READ_REG(REG) get the data from it without using like: #define READ_REG(REG) (*(REG))
But it's not an address, huart->Instance is an address, SR is a field in a structure the that huart->Instance points too
2023-12-13 12:45 PM - edited 2023-12-13 12:48 PM
In C++ the argument of READ_REG would be a reference, for example:
inline uint32_t READ_REG(volatile uint32_t ®)
{
return reg;
}
but all we have there is plain old C.
Why double layers of parentheses? Just because they did so.
2023-12-13 1:53 PM
So preprocessor treats like a function..
https://gcc.gnu.org/onlinedocs/gcc-4.7.4/cpp/Macro-Arguments.html
2023-12-13 4:31 PM
There is a better question - why does such macro exist at all? With what are they planning to hypothetically redefine these "future proof" macros? PCI_BusWrite()?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.