2012-05-08 3:08 AM
For my current project we are using a development board of powerAVR. It has a 3.5� TFT touchpanel with resolution 320x240, using 16bit FSMC bus for communication. But I need to have implement it on a 5.7� TFT with resolution 640x480.
We have been searching to find a suitable part which is FSMC compatible, but with no success till now. can anyone provide the details regarding the part number of the same.
The controller on the development board is STM32F103ZE and the display controller is SSD1963. It will be very appreciated if the display controller is the same.
2012-05-08 10:50 PM
For your Requirment IS64WV102416BLL will be sufficient.
2012-05-09 9:18 PM
AM-640480GTMQW-00H
2012-05-10 1:57 AM
Thanks for reply:-)
but i actually need a Touchpanel integrated TFT. LCD it should be 640x480, 5.7'' and 16bit FSMC compatible. if it is controlled by SSD1963 display controller it will be more helpful to me.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.