2012-09-27 3:13 PM
Hi, first of all thanks for reading this!
This is assembly code (gnu arm) for setting up the ST32F103 to make sound out the DAC. It works in 48mhz PLL mode, but not in What follows is the complete program, demonstrating the problem. Thanks again, -Peter B, RTOS engineer, shbobo.net
.thumb
.syntax unified
.equ STACKINIT, 0x2000C000
.equ RCC_CR, 0x40021000
.equ RCC_CFGR, 0x40021004
.equ RCC_APB1ENR, 0x4002101C
.equ GPIOA_CRL, 0x40010800
.equ DAC_BOUNDARY, 0x40007400
.equ DAC_DHR12R1, 0x40007408
@for ST32F103RCT6, uses pin PA4 (DAC)
@compiled with arm-elf-as or arm-linux-gnueabi-as
@-mcpu=cortex-m3 upload with ST-LINK_CLI.exe
@>>>>>>>>>>>>>>><<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<
@the following program sets up an external crystal
@at 8 megahertz, then sets up the PLL to multiply.
@it thus works at 48 megahertz (*6), and produces a saw
@waveform at the DAC output, done by the loop at the end.
@this is a distillation of a much larger program that at 48mhz,
@works with USB, adc, timer, dac, SYstick, and GPIO.
@but not at 72 mhz.
@the question is, if you comment out the following equate,
@why does it break at 72 megahertz (*9)???? please,
@comment/uncomment the next line about ''FORTYEIGHT''
.equ FORTYEIGHT, 1
vectors:
.word STACKINIT
.word initiate + 1
.word initiate + 1
.word initiate + 1
.word initiate + 1
.word initiate + 1
.word initiate + 1
.macro LODESTRA reg, val
ldr r1, =\reg @for setting
ldr r0, =\val @configurations
str r0, [r1] @in Mister ST
.endm
initiate:
LODESTRA RCC_CR, 0x00010081 @ HSEON
CRYSTAL_waiter:
ldr r1, = RCC_CR
ldr r1, [r1]
ldr r0, = 0x00020002 @ HSERDY
tst r1, r0
beq CRYSTAL_waiter
@NOTE THE FOLLOWING TWO POSSIBLE CONFIGURATIONS
.ifdef FORTYEIGHT
.equ CLOCKCONFIG, 0x0051FC00
@analyzed in bits:
@xxxx reserved
@x000 MCO off
@x101 USBPRE/1, PLL*6
@0001 PLL*6, HSE as source
@1111 ADC=AHB/8 APB2=AHB/16
@1100 APB1=AHB/2
@0000 0000
.else
.equ CLOCKCONFIG, 0x001DFD00
@analyzed in bits:
@xxxx reserved
@x000 MCO off
@x001 USBPRE/1.5, PLL*9
@1101 PLL*9, HSE as source
@1111 ADC=AHB/8 APB2=AHB/16
@1101 APB1=AHB/4
@0000 0000
.endif
LODESTRA RCC_CFGR, CLOCKCONFIG
LODESTRA RCC_CR, 0x01010081 @PLL ON
PLL_waiter:
ldr r1, = RCC_CR
ldr r1, [r1]
ldr r0, = 0x02020002 @PLL RDY
tst r1, r0
beq PLL_waiter
LODESTRA RCC_CFGR, (CLOCKCONFIG | 2) @ USE PLL as clock
LODESTRA RCC_APB1ENR, 0x20000000 @ DAC APB1 enable
LODESTRA GPIOA_CRL, 0x44004444 @ analog in for DAC
LODESTRA DAC_BOUNDARY, 0x00010001 @ turn on both DACs
1:
ldr r1, = DAC_DHR12R1
strh r0, [r1]
subs r0, r0, 1
b 1b @loop a saw waveform forever!
.end
#pll #pll #!bug #72mhz #pll-72mhz #pll
2012-09-27 3:36 PM
Doesn't appear to address wait states on the flash, or wait for the PLL source to become the system source.
The former will definitely give you headaches.2012-09-27 3:42 PM
Is there some rational to testing irrelevant bits here?
ldr r0, = 0x00020002 @ HSERDY ldr r0, = 0x02020002 @PLL RDY2012-09-27 5:34 PM
Hi, thanks for replying so quick. As regards waiting for the PLL source to settle, note the lines labeled ''PLL_waiter'' up until the ''beq PLL_waiter''. It is a while loop scheme to test until the RCC control register says PLL is ready. I hope that elucidates your question on the lines here, they are tst'ing the control register, and its cumulative state of HSE ready, then PLL ready. thanks again. -Peter B
Is there some rational to testing irrelevant bits here?ldr r0, = 0x00020002 @ HSERDY
ldr r0, = 0x02020002 @PLL RDY2012-09-27 5:39 PM
BTW, i think i can clarify one other thing. this code works great at 48mhz, so testing the bits that have already been tested is apparently, OK. it seems to be something about 72mhz that makes it break. I've ruled out anything electrical, because, as i said, the PLL works at 48mhz, and the 8mhz sans PLL definitely works too.
Wait states on flash? You can't mean that at 72mhz, a ''ldr ldr str'' type operation would break? Thanks again so much to clive1 and anyone else who can maybe try this code out and tell me i'm crazy!2012-09-27 7:02 PM
Thing is, if you test HSI RDY and you change upstream code you've created a bunch of dependencies.
FLASH, you need the equivalent to /* Enable Prefetch Buffer */ FLASH->ACR |= FLASH_ACR_PRFTBE; /* Flash 2 wait state */ FLASH->ACR &= (uint32_t)((uint32_t)~FLASH_ACR_LATENCY); FLASH->ACR |= (uint32_t)FLASH_ACR_LATENCY_2; And finally /* Wait till PLL is used as system clock source */ while ((RCC->CFGR & (uint32_t)RCC_CFGR_SWS) != (uint32_t)0x08); Perhaps some of it is not absolutely necessary, but adds predictability in terms of bringing up analogue parts with board-to-board variability, and then meshing gears as it transitions from one clock to another.2012-09-29 2:29 PM
Thanks to clive1 i got it going ( i think).
He was right, the prefetch buffer does need to be tweaked.A recommendation to newbies who want to master the literature on this product:read RM0008 (about STM32F103xx) AND read PM0075- programming manual specifically about flash memory. it has key morsels, such as all about the Access Control Register.to fix my code, i needed to add this macro call before configuring the PLL:LODESTRA FLASH_ACR, 0x31I still have a question.I originally was running the PLL at 48mhz, and i was not loading anything into the ACR, so it was maintaining the restart value of 0x30 (prefetch buffer enabled, no latency). why did it work at all when it should have been 0x31 (one wait state)? Actually, 72mhz sysclck works as well at 0x31 as 0x32 (one wait state versus two). That is confusing, because the PM0075 expressly states that 72mhz must have two wait states on the flash, as Clive1 said.Well, I'm going to keep the ACR at one wait state for now and see if anything bugs, but it sounds right, and USB is working so... thanks clive!2012-09-30 5:52 AM
The speed of the flash is effected by the voltage and temperature you run the processor at, ST rates it at around 24 MHz. I've run a couple of parts at 32 MHz without wait states, but haven't probed the limits, or tested over operational specs.
36 MHz might also work, but I wouldn't rely on it.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.